<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2346397#M28381</link>
    <description>&lt;P&gt;Could you show SIU_PCR configuration for those pins?&lt;/P&gt;</description>
    <pubDate>Tue, 07 Apr 2026 13:57:50 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2026-04-07T13:57:50Z</dc:date>
    <item>
      <title>GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2303881#M28312</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are configuring &lt;STRONG&gt;GPIO221 and GPIO222 as output pins&lt;/STRONG&gt; on an MCU with part number &lt;STRONG&gt;SPC5674FMVY3&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Observed behavior:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;The application is flashed into the board using a programmer.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;After flashing, when the &lt;STRONG&gt;programmer is removed&lt;/STRONG&gt;, &lt;STRONG&gt;GPIO221 and GPIO222 do not go high&lt;/STRONG&gt;.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;When the &lt;STRONG&gt;programmer remains connected&lt;/STRONG&gt;, GPIO221 and GPIO222 work correctly and go high.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Other GPIO output pins on the same board are functioning correctly&lt;/STRONG&gt; in both cases (with and without the programmer).&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Question:&lt;/STRONG&gt;&lt;BR /&gt;Why do only GPIO221 and GPIO222 fail to work in standalone mode, while other output pins function normally?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Narendra.C&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 15:14:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2303881#M28312</guid>
      <dc:creator>CNarendra</dc:creator>
      <dc:date>2026-01-30T15:14:43Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2304473#M28313</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a &lt;STRONG&gt;SPC5674FMVY3&lt;/STRONG&gt; MCU with &lt;STRONG&gt;3M17W &lt;/STRONG&gt;marking on the board.&lt;/P&gt;&lt;P&gt;As per below thread, Based on the marking, can you confirm if this&amp;nbsp;&lt;STRONG&gt;SPC5674FMVY3&amp;nbsp;part&amp;nbsp;&lt;/STRONG&gt;corresponds to &lt;STRONG&gt;Revision 2.3&lt;/STRONG&gt; of the MCU?&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/MPC5674F-Includes-eTPU-or-eTPU2/m-p/1913935" target="_blank" rel="noopener"&gt;MPC5674F Includes eTPU or eTPU2?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;As per the datasheet, GPIO220 and GPIO221 are expected to function only on &lt;EM&gt;&lt;STRONG&gt;Revision 2&lt;/STRONG&gt;&lt;/EM&gt; . We want to ensure our chip revision meets this requirement, as currently these GPIOs only work when the programmer is connected. but other GPIO223 is working fine&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image (3).png" style="width: 812px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375120i9DECA326CD250D8A/image-size/large?v=v2&amp;amp;px=999" role="button" title="image (3).png" alt="image (3).png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm the revision from the marking and any implications for GPIO functionality?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;Thanks&amp;nbsp;&lt;BR /&gt;Narendra.C&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234212"&gt;@Durga_Srinivasu&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Feb 2026 07:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2304473#M28313</guid>
      <dc:creator>CNarendra</dc:creator>
      <dc:date>2026-02-02T07:39:40Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2312612#M28323</link>
      <description>&lt;P&gt;Hi ,&lt;BR /&gt;&lt;BR /&gt;Kindly help on this,&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As per the &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;SIU.MIDR register&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt;, the current chip with us is &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;Revision 2&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt;. Hence, &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;GPIO221 and GPIO222 should be supported&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; as per the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Revision" style="width: 566px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375618i9DEE7B8605866E29/image-size/large?v=v2&amp;amp;px=999" role="button" title="SIU_MIDR_Register.png" alt="Revision" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Revision&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, these GPIOs work only when the debugger is connected and do not toggle in standalone mode. Please advise if any &lt;/SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;additional configuration, pin muxing, or errata&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN&gt; needs to be considered for these pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Narendra.C&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234212"&gt;@Durga_Srinivasu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 07:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2312612#M28323</guid>
      <dc:creator>CNarendra</dc:creator>
      <dc:date>2026-02-05T07:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2346394#M28380</link>
      <description>&lt;P&gt;eTPU2&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 13:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2346394#M28380</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-04-07T13:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO221 / GPIO222 Outputs are not working on MPC5674F when disconnected from programmer</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2346397#M28381</link>
      <description>&lt;P&gt;Could you show SIU_PCR configuration for those pins?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 13:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO221-GPIO222-Outputs-are-not-working-on-MPC5674F-when/m-p/2346397#M28381</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-04-07T13:57:50Z</dc:date>
    </item>
  </channel>
</rss>