<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ICST ERROR in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2333341#M28347</link>
    <description>&lt;P&gt;Using codewarrior V11.1 developed the MPC5644A program whith the ICST library. It runs normally in debug mode, but the program cannot run when offline. Looking forward to receiving your help.&lt;/P&gt;</description>
    <pubDate>Mon, 16 Mar 2026 08:11:51 GMT</pubDate>
    <dc:creator>JackW</dc:creator>
    <dc:date>2026-03-16T08:11:51Z</dc:date>
    <item>
      <title>ICST ERROR</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2333341#M28347</link>
      <description>&lt;P&gt;Using codewarrior V11.1 developed the MPC5644A program whith the ICST library. It runs normally in debug mode, but the program cannot run when offline. Looking forward to receiving your help.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Mar 2026 08:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2333341#M28347</guid>
      <dc:creator>JackW</dc:creator>
      <dc:date>2026-03-16T08:11:51Z</dc:date>
    </item>
    <item>
      <title>Re: ICST ERROR</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2333807#M28348</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;With provided failure analyzes is nearly impossible to tell where the issue is.&lt;/P&gt;
&lt;P&gt;Start with watchdogs and timers. Those are usually halted in debug mode. Once debug mode is left the timers will run and trigger events like exceptions, etc ...&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 17 Mar 2026 05:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2333807#M28348</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-03-17T05:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: ICST ERROR</title>
      <link>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2334416#M28351</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are other functions in my main program, such as ADC and serial communication, which can run normally offline as long as ICST is not called.&lt;/P&gt;&lt;P&gt;The ICST version is&amp;nbsp;e200Zx_ICST_RTMC_3.0.0&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 04:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/ICST-ERROR/m-p/2334416#M28351</guid>
      <dc:creator>JackW</dc:creator>
      <dc:date>2026-03-18T04:31:29Z</dc:date>
    </item>
  </channel>
</rss>