<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: FCCU error reporting integrity test (PLL) - NCF[32]</title>
    <link>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149729#M27876</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is there any &lt;STRONG&gt;Application note&lt;/STRONG&gt; which provides how we can inject failures for each NCF failures.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No. there is no such application note.&lt;/P&gt;
&lt;P&gt;The closest ones would be:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5284.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5284.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5259.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5259.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Aug 2025 05:14:40 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2025-08-11T05:14:40Z</dc:date>
    <item>
      <title>FCCU error reporting integrity test (PLL) - NCF[32]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2148462#M27861</link>
      <description>&lt;P&gt;I am currently working on the &lt;STRONG&gt;FCCU error reporting integrity check&lt;/STRONG&gt;. My goal is to verify that the error path—from the fault detection mechanism to the FCCU—is functioning correctly.&lt;/P&gt;&lt;P&gt;Under normal operation, I monitor &lt;STRONG&gt;FCCU NCF[32]&lt;/STRONG&gt; to detect if a &lt;STRONG&gt;PLL failure&lt;/STRONG&gt; is active.&lt;/P&gt;&lt;P&gt;However, during &lt;STRONG&gt;Power-On Tests (POT)&lt;/STRONG&gt;, I want to ensure that the error propagation path is working end-to-end. Specifically, I want to &lt;STRONG&gt;inject or simulate a PLL fault&lt;/STRONG&gt;, verify that it is correctly &lt;STRONG&gt;captured by the MEMU&lt;/STRONG&gt;, and ensure that it is then &lt;STRONG&gt;reported to the FCCU&lt;/STRONG&gt;. This confirms that the integrity of the fault detection and reporting path is intact.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Also, How can i inject PLL failure, so that i can verify the path of failure.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Aug 2025 12:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2148462#M27861</guid>
      <dc:creator>AshokSubramani</dc:creator>
      <dc:date>2025-08-07T12:01:09Z</dc:date>
    </item>
    <item>
      <title>Re: FCCU error reporting integrity test (PLL) - NCF[32]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149029#M27864</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Also, How can i inject PLL failure, so that i can verify the path of failure?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Since you did not share the device you are using I will answer generally.&lt;/P&gt;
&lt;P&gt;You can inject the fault in FCCU via NCFF&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1754640403628.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351538i93D8FEB2EF0EA8A6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1754640403628.png" alt="petervlna_0-1754640403628.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This will test FCCU reaction on fault.&lt;/P&gt;
&lt;P&gt;However if you want to test full reporting path. Simply&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I want to &lt;STRONG&gt;inject or simulate a PLL fault&lt;/STRONG&gt;, verify that it is correctly &lt;STRONG&gt;captured by the MEMU&lt;/STRONG&gt;, and ensure that it is then &lt;STRONG&gt;reported to the FCCU&lt;/STRONG&gt;.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;I ma confused here. MEMU has nothing to do with PLL loss of lock. It captures ECC events.&lt;/P&gt;
&lt;P&gt;Simply change your pll setting to get it out of lock and you will get the PLL fault NCF in FCCU. For example disconnect the XOSC on the board during runtime. Or reconfigure PLL to be out of VCO range.&lt;/P&gt;
&lt;P&gt;PLL can be is also monitored by CMU if selected as clock for that region.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 08:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149029#M27864</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-08-08T08:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: FCCU error reporting integrity test (PLL) - NCF[32]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149080#M27865</link>
      <description>&lt;P&gt;I am working on the MPC5746C, and as part of our ISO 26262 functional safety compliance, we need to verify the fault detection path for various modules including peripherals, RAM, Flash.&lt;/P&gt;&lt;P&gt;Specifically, during Power-On Testing (POT), we would like to simulate or inject faults to validate that the corresponding &lt;STRONG&gt;FCCU NCF channels&lt;/STRONG&gt; are capable of detecting and reporting those faults reliably. Is there any &lt;STRONG&gt;Application note&lt;/STRONG&gt; which provides how we can inject failures for each NCF failures.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AshokSubramani_0-1754643558475.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351550i0D877C96C38FAC3E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AshokSubramani_0-1754643558475.png" alt="AshokSubramani_0-1754643558475.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 09:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149080#M27865</guid>
      <dc:creator>AshokSubramani</dc:creator>
      <dc:date>2025-08-08T09:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: FCCU error reporting integrity test (PLL) - NCF[32]</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149729#M27876</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is there any &lt;STRONG&gt;Application note&lt;/STRONG&gt; which provides how we can inject failures for each NCF failures.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No. there is no such application note.&lt;/P&gt;
&lt;P&gt;The closest ones would be:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5284.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5284.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5259.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5259.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 05:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FCCU-error-reporting-integrity-test-PLL-NCF-32/m-p/2149729#M27876</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-08-11T05:14:40Z</dc:date>
    </item>
  </channel>
</rss>