<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5744P MCAL ISO26262 package integration issue</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091949#M27587</link>
    <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;From the link below,&amp;nbsp;I understood that RTD exe file is required for working with Tresos.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/EB-Tresos-config-S32K312/m-p/1774585" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/EB-Tresos-config-S32K312/m-p/1774585&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;and since this product line has no RTD, is it not possible to work with Tresos ? and so no possibility to configure&lt;/P&gt;</description>
    <pubDate>Tue, 06 May 2025 07:02:38 GMT</pubDate>
    <dc:creator>AndrewwDabach</dc:creator>
    <dc:date>2025-05-06T07:02:38Z</dc:date>
    <item>
      <title>MPC5744P MCAL ISO26262 package integration issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091414#M27582</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with MPC5744P with the e200z4 processors using the S32DS version 2.1.&lt;BR /&gt;Application - Industrial (Safety critical IEC61508)&lt;/P&gt;&lt;P&gt;Since the SDK was not safety certified, it was suggested to used the ISO26262 MCAL drivers, which was created for the AUTOSAR project [1]. But in its integration manual, it is mentioned that I have to use Tresos tool to modify and generate MCAL component configuration [2]. Does it mean that I cannot use the Processor Export tool for generating configurations here when using the ISO26262 MCAL package. Could you please clarify? and also on how to use the ISO MCAL package in the non-AUTOSAR environment?&lt;/P&gt;&lt;P&gt;[1] &lt;A href="https://community.nxp.com/t5/MPC5xxx/Safety-certification-for-the-gcc-compiler-in-S32DS-for-power/m-p/2073322/highlight/false#M27497" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/Safety-certification-for-the-gcc-compiler-in-S32DS-for-power/m-p/2073322/highlight/false#M27497&lt;/A&gt;&lt;BR /&gt;[2] AUTOSAR_MCAL_SPI_IM Section 5.3 and also AUTOSAR_MCAL_SPI_UM Section 3.6.2 pdfs&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 12:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091414#M27582</guid>
      <dc:creator>AndrewwDabach</dc:creator>
      <dc:date>2025-05-05T12:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P MCAL ISO26262 package integration issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091553#M27583</link>
      <description>&lt;P&gt;Yes, correct.&lt;/P&gt;
&lt;P&gt;On this product line there were no RTD and there were 2 options: SDK that is free of charge and MCAL is not for free and customer must other AUTOSAR tools to use it.&lt;/P&gt;
&lt;P&gt;1) Yes, Tresos must be used.&lt;/P&gt;
&lt;P&gt;2) Unfortunately Processor Expert cannot be used.&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 16:10:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091553#M27583</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-05-05T16:10:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P MCAL ISO26262 package integration issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091904#M27585</link>
      <description>&lt;P&gt;Thank you for your response. Could you kindly clarify what does "MCAL is not for free" means ? I am confused because I was able to download the ISO MCAL package and the Tresos tool with license from the NXP websites for free. Is there something more I should be looking into?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW574XP-SMCL401E" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW574XP-SMCL401E&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 05:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091904#M27585</guid>
      <dc:creator>AndrewwDabach</dc:creator>
      <dc:date>2025-05-06T05:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P MCAL ISO26262 package integration issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091937#M27586</link>
      <description>&lt;P&gt;I am apologizing, I wanted to write "MCAL may not be for free"&lt;/P&gt;
&lt;P&gt;If you see following table, most of MCAL releases is now free of charge, icluding MCAL for MPC5744P:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/autosar:AUTOSAR-HOME" target="_blank"&gt;https://www.nxp.com/design/design-center/software/automotive-software-and-tools/autosar:AUTOSAR-HOME&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 06:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091937#M27586</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-05-06T06:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P MCAL ISO26262 package integration issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091949#M27587</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;From the link below,&amp;nbsp;I understood that RTD exe file is required for working with Tresos.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/EB-Tresos-config-S32K312/m-p/1774585" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/EB-Tresos-config-S32K312/m-p/1774585&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;and since this product line has no RTD, is it not possible to work with Tresos ? and so no possibility to configure&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 07:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-MCAL-ISO26262-package-integration-issue/m-p/2091949#M27587</guid>
      <dc:creator>AndrewwDabach</dc:creator>
      <dc:date>2025-05-06T07:02:38Z</dc:date>
    </item>
  </channel>
</rss>