<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5566 FlexCAN</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207493#M27</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you already&amp;nbsp; read &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN1798.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN1798.pdf&lt;/A&gt; (CAN Bit Timing Requirements)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2012 09:53:51 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2012-10-25T09:53:51Z</dc:date>
    <item>
      <title>MPC5566 FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207491#M25</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could anyone please explain how to calculate the baudrate for the FlexCAN on the MPC5566, currently im lost,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a 8Mz Crystal and require&amp;nbsp; buadrate of 1Mz&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Oct 2012 15:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207491#M25</guid>
      <dc:creator>r_james14</dc:creator>
      <dc:date>2012-10-03T15:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5566 FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207492#M26</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Checkout section 22.4.5.4 "Protocol Timing" of the MPC5566 Reference Manual.&lt;/P&gt;&lt;P&gt;The relevant parameters are set in the CAN Control Register (CAN_CR), described in section 22.3.3.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an example:&lt;/P&gt;&lt;P&gt;To get a bit rate of 1MHz, choose:&lt;/P&gt;&lt;P&gt;CLK_SRC = 0 (crystal source)&lt;/P&gt;&lt;P&gt;PRESDIV = 0&lt;/P&gt;&lt;P&gt;This will set the time quanta frequency, ftq, to 8 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, choose a combination of PROPSEG, PSEG1 and PSEG2 to give 8 'time quanta' per bit time&lt;/P&gt;&lt;P&gt;Bit rate will then be &lt;/P&gt;&lt;P&gt;&amp;nbsp; ftq / num time quanta = 8 Mhz / 8 = 1Mhz, as desired&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 09:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207492#M26</guid>
      <dc:creator>chrism</dc:creator>
      <dc:date>2012-10-23T09:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5566 FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207493#M27</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you already&amp;nbsp; read &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN1798.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN1798.pdf&lt;/A&gt; (CAN Bit Timing Requirements)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2012 09:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5566-FlexCAN/m-p/207493#M27</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2012-10-25T09:53:51Z</dc:date>
    </item>
  </channel>
</rss>