<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5606B BAM Serial Communication in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-BAM-Serial-Communication/m-p/494153#M2680</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just read about the included Boot Assist Module in MPC5606B. I understand that I have to set the FAB and ABS pins accordingly to disable booting from internal flash and make use of the Boot Assist Module instead.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?&lt;/P&gt;&lt;P&gt;Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?&lt;/P&gt;&lt;P&gt;For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Feb 2016 22:00:06 GMT</pubDate>
    <dc:creator>fscheidl</dc:creator>
    <dc:date>2016-02-06T22:00:06Z</dc:date>
    <item>
      <title>MPC5606B BAM Serial Communication</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-BAM-Serial-Communication/m-p/494153#M2680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just read about the included Boot Assist Module in MPC5606B. I understand that I have to set the FAB and ABS pins accordingly to disable booting from internal flash and make use of the Boot Assist Module instead.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?&lt;/P&gt;&lt;P&gt;Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?&lt;/P&gt;&lt;P&gt;For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Feb 2016 22:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-BAM-Serial-Communication/m-p/494153#M2680</guid>
      <dc:creator>fscheidl</dc:creator>
      <dc:date>2016-02-06T22:00:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B BAM Serial Communication</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-BAM-Serial-Communication/m-p/494154#M2681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?&lt;/P&gt;&lt;P&gt;- Yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?&lt;/P&gt;&lt;P&gt;- Yes:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59426iF8C6CD85B57C7D1B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?&lt;/P&gt;&lt;P&gt;- Yes:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59460i0449B573A5AAD813/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 11:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-BAM-Serial-Communication/m-p/494154#M2681</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-02-08T11:44:42Z</dc:date>
    </item>
  </channel>
</rss>