<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5775B internal temperature sensing in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1960924#M26704</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to calculate the temperature using the MCU's internal temperature sensors. I read the ADC voltage values for the local bandgap, TempSense-1, and TempSense-2, and used the formula provided in the reference manual. I also read the calibration values from the UTEST memory:&lt;BR /&gt;- Sensor 0 Cal A: 237&lt;BR /&gt;- Sensor 0 Cal B: 54&lt;BR /&gt;- Sensor 1 Cal A: 127&lt;BR /&gt;- Sensor 1 Cal B: 1&lt;/P&gt;&lt;P&gt;Based on these values, I'm calculating a temperature. However, when compared with a temperature monitoring camera, the readings show a 5-10°C difference (lower in my calculation). Additionally, the MCU is resetting when the temperature reaches 180°C based on my calculations, but the reference manual indicates that the MCU should reset at 150°C.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Sep 2024 16:13:47 GMT</pubDate>
    <dc:creator>bharathn3402</dc:creator>
    <dc:date>2024-09-24T16:13:47Z</dc:date>
    <item>
      <title>MPC5775B internal temperature sensing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1960924#M26704</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to calculate the temperature using the MCU's internal temperature sensors. I read the ADC voltage values for the local bandgap, TempSense-1, and TempSense-2, and used the formula provided in the reference manual. I also read the calibration values from the UTEST memory:&lt;BR /&gt;- Sensor 0 Cal A: 237&lt;BR /&gt;- Sensor 0 Cal B: 54&lt;BR /&gt;- Sensor 1 Cal A: 127&lt;BR /&gt;- Sensor 1 Cal B: 1&lt;/P&gt;&lt;P&gt;Based on these values, I'm calculating a temperature. However, when compared with a temperature monitoring camera, the readings show a 5-10°C difference (lower in my calculation). Additionally, the MCU is resetting when the temperature reaches 180°C based on my calculations, but the reference manual indicates that the MCU should reset at 150°C.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 16:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1960924#M26704</guid>
      <dc:creator>bharathn3402</dc:creator>
      <dc:date>2024-09-24T16:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B internal temperature sensing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1962434#M26716</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The sensors measure the temperature inside the silicon. And you measure it on the surface.&lt;/P&gt;
&lt;P&gt;With 150C are you referring to Junction operating temperature range?&lt;/P&gt;
&lt;P&gt;Where do you read that at 150C you will get reset?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 07:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1962434#M26716</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-09-26T07:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B internal temperature sensing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1962588#M26717</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I measured the internal temperature sensor value using the ADC, which provides the junction temperature. The MCU's operating temperature range is from -40°C to 150°C, and the reset condition is mentioned in the &lt;STRONG&gt;PMC_REE_TD&lt;/STRONG&gt; register.&lt;/P&gt;&lt;P&gt;I measured the MCU's internal sensor ADC values and performed calculations as outlined in the reference manual. I validated this with a thermal camera by measuring the MCU surface temperature. When the surface temperature reached 180°C, the MCU reset, and once it cooled down, it returned to normal operation.&lt;/P&gt;&lt;P&gt;Do you have any idea about the ADC values generated at certain temperatures for a 14-bit ADC? Also, I need more information regarding the ADC reference voltages.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 09:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1962588#M26717</guid>
      <dc:creator>bharathn3402</dc:creator>
      <dc:date>2024-09-26T09:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B internal temperature sensing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1964993#M26754</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Do you have any idea about the ADC values generated at certain temperatures for a 14-bit ADC?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No, as each chip has unique calibration values. There is no point to have such&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Also, I need more information regarding the ADC reference voltages.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Not sure what you need. All available specifications are in datasheet.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 07:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/1964993#M26754</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-10-01T07:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5775B internal temperature sensing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/2001203#M27006</link>
      <description>&lt;P&gt;Hai&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/13836"&gt;@petervlna&lt;/a&gt;&amp;nbsp;, Can i have an example code for MPC5775B&amp;nbsp;ADC Initialization, Reading for SDK Peripheral Abstraction Layer for Analog to Digital Converter (ADC PAL)&lt;BR /&gt;Repository: SDK_S32_PA_15 .&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 14:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5775B-internal-temperature-sensing/m-p/2001203#M27006</guid>
      <dc:creator>bharathn3402</dc:creator>
      <dc:date>2024-11-25T14:41:24Z</dc:date>
    </item>
  </channel>
</rss>