<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debugging after reset automatically using lauterbach debugger in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Debugging-after-reset-automatically-using-lauterbach-debugger/m-p/1953313#M26667</link>
    <description>&lt;P&gt;I made a project configuration using CMM script to test my software on MPC5777. In the software there is a component that make a reset so it make the debug failed. In this case, I need your support through an example of script CMM that include this commands SYStem.Option.ResetDetection ; SYStem.Option.RESetBehavior to reconnect the debugger automatically to the selected Core ( in my case Core 2 IOP )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 09:01:38 GMT</pubDate>
    <dc:creator>Ahmed_BEN_LAKHEL1234</dc:creator>
    <dc:date>2024-09-12T09:01:38Z</dc:date>
    <item>
      <title>Debugging after reset automatically using lauterbach debugger</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debugging-after-reset-automatically-using-lauterbach-debugger/m-p/1953313#M26667</link>
      <description>&lt;P&gt;I made a project configuration using CMM script to test my software on MPC5777. In the software there is a component that make a reset so it make the debug failed. In this case, I need your support through an example of script CMM that include this commands SYStem.Option.ResetDetection ; SYStem.Option.RESetBehavior to reconnect the debugger automatically to the selected Core ( in my case Core 2 IOP )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 09:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debugging-after-reset-automatically-using-lauterbach-debugger/m-p/1953313#M26667</guid>
      <dc:creator>Ahmed_BEN_LAKHEL1234</dc:creator>
      <dc:date>2024-09-12T09:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging after reset automatically using lauterbach debugger</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debugging-after-reset-automatically-using-lauterbach-debugger/m-p/1954014#M26674</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I have already posted my thoughts at:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Zephyr-Project/Debugging-after-reset-automatically-using-lauterbach-debugger/td-p/1953307" target="_blank"&gt;https://community.nxp.com/t5/Zephyr-Project/Debugging-after-reset-automatically-using-lauterbach-debugger/td-p/1953307&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I suggest to continue with just one thread.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 13 Sep 2024 06:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debugging-after-reset-automatically-using-lauterbach-debugger/m-p/1954014#M26674</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-09-13T06:53:25Z</dc:date>
    </item>
  </channel>
</rss>