<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Need help with eMIOS</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Need-help-with-eMIOS/m-p/493453#M2647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no simulator for eMIOS timer, as it is relatively simple peripheral in comparison to eTPU. &lt;/P&gt;&lt;P&gt;I could recommend AN2865, sections 18 and 19:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also following document could be useful to see (at least to know it exists):&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/EB651.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/EB651.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure what would like to know SoC connection but if you ask about interconnection between eTPU and eMIOS, there is STAC bus and time bases synchronization:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;21.3.5.3 STAC Interface&lt;/LI&gt;&lt;LI&gt;21.3.5.4 GTBE - Global Time Base Enable&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this question aims to pad to module routing then I would link to SIU module’s PCR registers configuring particular pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 May 2016 08:05:37 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-05-25T08:05:37Z</dc:date>
    <item>
      <title>Need help with eMIOS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-help-with-eMIOS/m-p/493452#M2646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;I will be working on MPC5676R to design a controller for the BLDC motor.&lt;/P&gt;&lt;P&gt;I need help with the eMIOS.&lt;/P&gt;&lt;P&gt;I have the following question:&lt;/P&gt;&lt;P&gt;How is it connected with the SoC?&lt;/P&gt;&lt;P&gt;Is there any interface required with eMIOS and eTPU?&lt;/P&gt;&lt;P&gt;Are there any simulators on which i can practice programming the eMIOS?&lt;/P&gt;&lt;P&gt;Code Warrior can be used for eTPU only.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 May 2016 09:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-help-with-eMIOS/m-p/493452#M2646</guid>
      <dc:creator>snehakalkhair</dc:creator>
      <dc:date>2016-05-23T09:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with eMIOS</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-help-with-eMIOS/m-p/493453#M2647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no simulator for eMIOS timer, as it is relatively simple peripheral in comparison to eTPU. &lt;/P&gt;&lt;P&gt;I could recommend AN2865, sections 18 and 19:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also following document could be useful to see (at least to know it exists):&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/EB651.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/EB651.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure what would like to know SoC connection but if you ask about interconnection between eTPU and eMIOS, there is STAC bus and time bases synchronization:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;21.3.5.3 STAC Interface&lt;/LI&gt;&lt;LI&gt;21.3.5.4 GTBE - Global Time Base Enable&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this question aims to pad to module routing then I would link to SIU module’s PCR registers configuring particular pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 08:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-help-with-eMIOS/m-p/493453#M2647</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-05-25T08:05:37Z</dc:date>
    </item>
  </channel>
</rss>