<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programming GPIO in MPC5668G in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Programming-GPIO-in-MPC5668G/m-p/493267#M2628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please refer to the following posted example; &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="11363" data-containertype="14" data-objectid="329563" data-objecttype="102" href="https://community.freescale.com/docs/DOC-329563"&gt;https://community.freescale.com/docs/DOC-329563&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It gives you basic demo code. It also set one pin to GPIO output and toggle it within timer interrupt. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To set the pin as input you need to set the SIU.PCR[x].IBE bit and read the pad level from the respective SIU.GPDI[x] register.&lt;/P&gt;&lt;P&gt;For example like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIU.PCR[16].R = 0x0200;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set PB0 as GPIO output&lt;/P&gt;&lt;P&gt;SIU.PCR[17].R = 0x0103;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set PB1 as GPIO input, pull ups enabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// if PB[0] pin is high then set PB[1] high, else put it low&lt;/P&gt;&lt;P&gt;if(SIU.GPDI[16].R) SIU.GPDO[17].R = 0x1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;else SIU.GPDO[17].R = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jan 2016 07:50:32 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-01-18T07:50:32Z</dc:date>
    <item>
      <title>Programming GPIO in MPC5668G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Programming-GPIO-in-MPC5668G/m-p/493266#M2627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am new to using this MCU. How can i program a GPIO pin to act as an input and output? For ex to read value of led port and write the value into a led port?&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ravikiran&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 13:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Programming-GPIO-in-MPC5668G/m-p/493266#M2627</guid>
      <dc:creator>ravikiranbhairu</dc:creator>
      <dc:date>2016-01-15T13:18:05Z</dc:date>
    </item>
    <item>
      <title>Re: Programming GPIO in MPC5668G</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Programming-GPIO-in-MPC5668G/m-p/493267#M2628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please refer to the following posted example; &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="11363" data-containertype="14" data-objectid="329563" data-objecttype="102" href="https://community.freescale.com/docs/DOC-329563"&gt;https://community.freescale.com/docs/DOC-329563&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It gives you basic demo code. It also set one pin to GPIO output and toggle it within timer interrupt. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To set the pin as input you need to set the SIU.PCR[x].IBE bit and read the pad level from the respective SIU.GPDI[x] register.&lt;/P&gt;&lt;P&gt;For example like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIU.PCR[16].R = 0x0200;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set PB0 as GPIO output&lt;/P&gt;&lt;P&gt;SIU.PCR[17].R = 0x0103;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set PB1 as GPIO input, pull ups enabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// if PB[0] pin is high then set PB[1] high, else put it low&lt;/P&gt;&lt;P&gt;if(SIU.GPDI[16].R) SIU.GPDO[17].R = 0x1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;else SIU.GPDO[17].R = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 07:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Programming-GPIO-in-MPC5668G/m-p/493267#M2628</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-01-18T07:50:32Z</dc:date>
    </item>
  </channel>
</rss>