<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 MPC5748G DCF</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-DCF/m-p/1910929#M25976</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i see the MPC5748G reference manual , about the&amp;nbsp; UTEST Memory Map section.&lt;/P&gt;&lt;P&gt;the address 0x004000C0 is&amp;nbsp;Soft DCF Record Start Address;&lt;/P&gt;&lt;P&gt;the address 0x00400300 is DCF Start Record;&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400308 is Reserved;&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400348 is&amp;nbsp;DCF Records;&lt;/P&gt;&lt;P&gt;It makes me wonder , if there has some different between the&amp;nbsp;Soft DCF Record and DCF&amp;nbsp;Record ?&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400308 is reserved , can i write something into this area?&lt;/P&gt;</description>
    <pubDate>Thu, 18 Jul 2024 02:51:13 GMT</pubDate>
    <dc:creator>haiyang</dc:creator>
    <dc:date>2024-07-18T02:51:13Z</dc:date>
    <item>
      <title>MPC5748G DCF</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-DCF/m-p/1910929#M25976</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i see the MPC5748G reference manual , about the&amp;nbsp; UTEST Memory Map section.&lt;/P&gt;&lt;P&gt;the address 0x004000C0 is&amp;nbsp;Soft DCF Record Start Address;&lt;/P&gt;&lt;P&gt;the address 0x00400300 is DCF Start Record;&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400308 is Reserved;&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400348 is&amp;nbsp;DCF Records;&lt;/P&gt;&lt;P&gt;It makes me wonder , if there has some different between the&amp;nbsp;Soft DCF Record and DCF&amp;nbsp;Record ?&lt;/P&gt;&lt;P&gt;the address&amp;nbsp;0x00400308 is reserved , can i write something into this area?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 02:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-DCF/m-p/1910929#M25976</guid>
      <dc:creator>haiyang</dc:creator>
      <dc:date>2024-07-18T02:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G DCF</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-DCF/m-p/1910979#M25978</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;It makes me wonder , if there has some different between the Soft DCF Record and DCF Record ?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Those are the marks for SSCM machine to read and copy data to correct locations.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;the address 0x00400308 is reserved , can i write something into this area?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No. You will write DCFs to :&lt;/P&gt;
&lt;P&gt;0x00400348 -- 0x00400FFF 3256 DCF Records&lt;BR /&gt;0x00401000 --0x00403FFF 12288 Reserved for customer OTP data&lt;/P&gt;
&lt;P&gt;Avoid write to reserved areas at all.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 04:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-DCF/m-p/1910979#M25978</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-07-18T04:23:09Z</dc:date>
    </item>
  </channel>
</rss>