<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: error during Flash  programming 5777C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1910730#M25972</link>
    <description>Hi,&lt;BR /&gt;At that time, we have given 5V to a pin instead of 3.3V. So, that caused problem when trying to program the code. Later, we verified the supply levels to all pins and rectified our mistake. After that, this issue is resolved.&lt;BR /&gt;But, sometimes, I get this error during flash programming, due to improper/loose connection of PE device cable / power supply not enough..</description>
    <pubDate>Wed, 17 Jul 2024 18:06:01 GMT</pubDate>
    <dc:creator>San_96</dc:creator>
    <dc:date>2024-07-17T18:06:01Z</dc:date>
    <item>
      <title>error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396395#M20089</link>
      <description>&lt;P&gt;I am unable to dump program to the card.&lt;/P&gt;&lt;P&gt;MPC5777C controller,&lt;/P&gt;&lt;P&gt;S32DS V1.2 IDE&lt;/P&gt;&lt;P&gt;PE micro USB multilink&lt;/P&gt;&lt;P&gt;While I try to dump the program, the below error is shown.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Initializing.&lt;BR /&gt;MPC577xC Device detected.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;BR /&gt;&lt;BR /&gt;Initializing.&lt;BR /&gt;MPC577xC Device detected.&lt;BR /&gt;Initialized.&lt;BR /&gt;&lt;BR /&gt;;version 1.04, 12/13/2016, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32DS-for-Power-v1-2-Error-loading-programming-algorithm-load/m-p/www.pemicro.com" target="test_blank" rel="nofollow noopener noreferrer"&gt;www.pemicro.com&lt;/A&gt; [5777C_8meg_highspeed]&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;;begin_cs device=$30800000, length=$00800000, ram=$00300000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Loading programming algorithm ... &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;Error loading .PCP file&lt;/FONT&gt; : C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048\win32\gdi\P&amp;amp;E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp at address &lt;/STRONG&gt;&lt;STRONG&gt;00300001&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Error loading programming algorithm - load aborted. &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Error occurred during Flash programming.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;And then Starting reset script.....&lt;/P&gt;&lt;P&gt;After some time, one error pop-up is shown as Flash programming error. terminating debug session.&lt;/P&gt;&lt;P&gt;The PE micro multilink and S32DS V1.2 IDE, I use, works well with other cards with MCU 5567, 5777. With this card only it is showing error. I checked all hardware connections. Everything is perfect as I designed the previous cards. With this card, things are not at all moving further. Need help. &lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 08:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396395#M20089</guid>
      <dc:creator>San_96</dc:creator>
      <dc:date>2022-01-11T08:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396699#M20096</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I've never seen this issue before.&lt;/P&gt;
&lt;P&gt;1. Please check if the &lt;STRONG&gt;nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp&lt;/STRONG&gt; file is in the specified folder.&lt;/P&gt;
&lt;P&gt;2. Please update the PEMicro plugin.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 09:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396699#M20096</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2022-01-10T09:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396710#M20098</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I checked the file. It is there in path.&amp;nbsp;&lt;/P&gt;&lt;P&gt;PEmicro is working properly for other project cards of MPC5777C same batch&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 10:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1396710#M20098</guid>
      <dc:creator>San_96</dc:creator>
      <dc:date>2022-01-10T10:30:07Z</dc:date>
    </item>
    <item>
      <title>Re: error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1397326#M20105</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;What comes to my mind. I sometimes have issue programming SPC5777C when its flash it is not erased first. Try to erase flash, once it is cleared, program it.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 10:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1397326#M20105</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2022-01-11T10:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1909964#M25964</link>
      <description>&lt;P&gt;Hello.&lt;BR /&gt;I have exactly the same problem.&lt;BR /&gt;S32 design studio, PE plugin and Multilink firmware are up-to-date.&lt;BR /&gt;Was any solution founded last time?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 17:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1909964#M25964</guid>
      <dc:creator>IvanIvanenkoTechSAT</dc:creator>
      <dc:date>2024-07-16T17:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: error during Flash  programming 5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1910730#M25972</link>
      <description>Hi,&lt;BR /&gt;At that time, we have given 5V to a pin instead of 3.3V. So, that caused problem when trying to program the code. Later, we verified the supply levels to all pins and rectified our mistake. After that, this issue is resolved.&lt;BR /&gt;But, sometimes, I get this error during flash programming, due to improper/loose connection of PE device cable / power supply not enough..</description>
      <pubDate>Wed, 17 Jul 2024 18:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/error-during-Flash-programming-5777C/m-p/1910730#M25972</guid>
      <dc:creator>San_96</dc:creator>
      <dc:date>2024-07-17T18:06:01Z</dc:date>
    </item>
  </channel>
</rss>