<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックPWM frequency calculation</title>
    <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1864192#M25459</link>
    <description>&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;I would like to ask how the PWM frequency of MPC5744P is calculated.&lt;/P&gt;&lt;P&gt;The following figure shows the parameters I configured, where the frequency of MOTC_CLK is 200MHz,PWM_CLK is MOTC_CLK's 16-frequency division is 12.5MHz. The reload point of channel 0 of PWM is 4096, and the initial point is 0. According to the calculation, it should be 200MHz/16/4096=3.05KHz, but the actual measurement is only 2.4KHz, which is within the error range or there is a problem with my calculation?&lt;/P&gt;</description>
    <pubDate>Mon, 13 May 2024 08:09:58 GMT</pubDate>
    <dc:creator>Wen666</dc:creator>
    <dc:date>2024-05-13T08:09:58Z</dc:date>
    <item>
      <title>PWM frequency calculation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1864192#M25459</link>
      <description>&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;I would like to ask how the PWM frequency of MPC5744P is calculated.&lt;/P&gt;&lt;P&gt;The following figure shows the parameters I configured, where the frequency of MOTC_CLK is 200MHz,PWM_CLK is MOTC_CLK's 16-frequency division is 12.5MHz. The reload point of channel 0 of PWM is 4096, and the initial point is 0. According to the calculation, it should be 200MHz/16/4096=3.05KHz, but the actual measurement is only 2.4KHz, which is within the error range or there is a problem with my calculation?&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 08:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1864192#M25459</guid>
      <dc:creator>Wen666</dc:creator>
      <dc:date>2024-05-13T08:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: PWM frequency calculation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1864980#M25468</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;calculation is correct, but note max MOTC_CLK can be 160MHz. As you selected PLL0 for MOTC_CLK, most probably PLL0 is set to 160MHz. With this value you get 2,4KHz with your calculation.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 06:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1864980#M25468</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-05-14T06:07:41Z</dc:date>
    </item>
    <item>
      <title>Re: PWM frequency calculation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1865778#M25480</link>
      <description>&lt;P&gt;OK,thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 01:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/PWM-frequency-calculation/m-p/1865778#M25480</guid>
      <dc:creator>Wen666</dc:creator>
      <dc:date>2024-05-15T01:26:37Z</dc:date>
    </item>
  </channel>
</rss>