<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5744 UART in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854376#M25373</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can also refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5744P-PinToggleStationery-S32DS-1-0/ta-p/1106644" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5744P-PinToggleStationery-S32DS-1-0/ta-p/1106644&lt;/A&gt;&lt;BR /&gt;It uses printf as well.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 25 Apr 2024 06:30:27 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-04-25T06:30:27Z</dc:date>
    <item>
      <title>MPC5744 UART</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854239#M25369</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I tried to use the following link to do printf experiments,&lt;BR /&gt;**&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/How-to-use-printf-function-in-S32DS-for-Power-Architecture-using/ta-p/1118901" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/How-to-use-printf-function-in-S32DS-for-Power-Architecture-using/ta-p/1118901&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However, during the establishment process, an error occurred in the established HW_Init(), and err= ReadUARTN(Buffer, 1u);&lt;/P&gt;&lt;P&gt;have anyone can tell me which part is problematic?&lt;/P&gt;&lt;P&gt;(Im base on SPI example to add this functions.)&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 03:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854239#M25369</guid>
      <dc:creator>gary1232</dc:creator>
      <dc:date>2024-04-25T03:20:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 UART</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854376#M25373</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can also refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5744P-PinToggleStationery-S32DS-1-0/ta-p/1106644" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5744P-PinToggleStationery-S32DS-1-0/ta-p/1106644&lt;/A&gt;&lt;BR /&gt;It uses printf as well.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 06:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854376#M25373</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-04-25T06:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744 UART</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854485#M25376</link>
      <description>&lt;P&gt;hi, peter&lt;/P&gt;&lt;P&gt;thank your reply.&lt;/P&gt;&lt;P&gt;i try your suggestion example to my board, but when i build the project... its show..-&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="gary1232_1-1714031243654.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275798i568047C7C6EAAA31/image-size/medium?v=v2&amp;amp;px=400" role="button" title="gary1232_1-1714031243654.png" alt="gary1232_1-1714031243654.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;how can i do...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 07:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-UART/m-p/1854485#M25376</guid>
      <dc:creator>gary1232</dc:creator>
      <dc:date>2024-04-25T07:48:47Z</dc:date>
    </item>
  </channel>
</rss>