<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5743 CAN interrupt</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5743-CAN-interrupt/m-p/1847116#M25300</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there is no difference in interrupt usage between CAN instances, except of different ISR vector numbers. What does "&lt;SPAN&gt;The program will get stuck in the receive interrupt" mean in fact. Does it mean interrupt is repeatedly called? If yes, be sure interrupt flag is properly cleared.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Apr 2024 12:06:49 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-04-15T12:06:49Z</dc:date>
    <item>
      <title>MPC5743 CAN interrupt</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5743-CAN-interrupt/m-p/1846437#M25286</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I have a total of three CAN communications, CAN2 uses interrupt reception, I use the same configuration to receive interrupts to CAN0, CAN1. The program will get stuck in the receive interrupt, what is the cause of this, and what is the difference between CAN2 and other CAN receive interrupt configurations&lt;/P&gt;</description>
      <pubDate>Sat, 13 Apr 2024 02:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5743-CAN-interrupt/m-p/1846437#M25286</guid>
      <dc:creator>xuan</dc:creator>
      <dc:date>2024-04-13T02:42:17Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5743 CAN interrupt</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5743-CAN-interrupt/m-p/1847116#M25300</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;there is no difference in interrupt usage between CAN instances, except of different ISR vector numbers. What does "&lt;SPAN&gt;The program will get stuck in the receive interrupt" mean in fact. Does it mean interrupt is repeatedly called? If yes, be sure interrupt flag is properly cleared.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 12:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5743-CAN-interrupt/m-p/1847116#M25300</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-04-15T12:06:49Z</dc:date>
    </item>
  </channel>
</rss>