<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5744p censorship</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831905#M25114</link>
    <description>&lt;P&gt;Hello Petervlna,&lt;BR /&gt;Thank you for your response&lt;BR /&gt;I'm using S32 design studio IDE, GCC compiler.&lt;BR /&gt;Does it make any difference ? as I'm trying to flash a new file with entering the password at the GDB server parameter and it always fails.&lt;/P&gt;</description>
    <pubDate>Wed, 20 Mar 2024 09:28:26 GMT</pubDate>
    <dc:creator>abdelrhman</dc:creator>
    <dc:date>2024-03-20T09:28:26Z</dc:date>
    <item>
      <title>MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831280#M25104</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;I'm using MPC5744p, I flashed the following array,&lt;BR /&gt;{0x55555555, 0x0100000C, 0x55555555, 0x01000008, 0x55555555, 0x01000004},&lt;BR /&gt;in the UTest memory section at address starting from 0x00400208.&lt;BR /&gt;the array data means that securing the microcontroller is enabled since the DCF record&amp;nbsp;NVSCI is programmed by 0x5555555 other than the default value 55AA55AA. and accordingly, as expected, the microcontroller is now secured. I'm expecting that the uncensor password will be 0x5555555555555555 since the Non-Volatile Password Low (NVPWDL) and Non-Volatile&lt;BR /&gt;Password High (NVPWDH) are configured by 0x 55555555 and 0x55555555. However, when I tried to uncensor the microcontroller using this password, I couldn't connect to it duo to wrong password.&lt;BR /&gt;&lt;BR /&gt;My question is&amp;nbsp;&lt;BR /&gt;is the uncensor password, 0x5555555555555555, wrong?&amp;nbsp;&lt;BR /&gt;If yes, how I can calculate the correct password based on the flashed array ?&lt;BR /&gt;If no, is there something else missing ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks in advance&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Mar 2024 15:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831280#M25104</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2024-03-19T15:43:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831805#M25111</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Password seem to me valid.&lt;/P&gt;
&lt;P&gt;I would suspect the way you enter the password.&lt;/P&gt;
&lt;P&gt;I have posted guide for it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5744P-Censorship-programing-with-Lauterbach/ta-p/1113543" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5744P-Censorship-programing-with-Lauterbach/ta-p/1113543&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 08:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831805#M25111</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-03-20T08:27:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831905#M25114</link>
      <description>&lt;P&gt;Hello Petervlna,&lt;BR /&gt;Thank you for your response&lt;BR /&gt;I'm using S32 design studio IDE, GCC compiler.&lt;BR /&gt;Does it make any difference ? as I'm trying to flash a new file with entering the password at the GDB server parameter and it always fails.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 09:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1831905#M25114</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2024-03-20T09:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1832679#M25119</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sorry I am not familiar with S32DS and these low cost debuggers.&lt;/P&gt;
&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159987"&gt;@jiri_kral&lt;/a&gt; do we have guide for Censoring / unlocking MPC devices via S32DS?&lt;/P&gt;
&lt;P&gt;In advance could you specify which debugger and S32DS are you using?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 07:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1832679#M25119</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-03-21T07:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1832690#M25120</link>
      <description>&lt;P&gt;I'm using openSDA Embedded Debug - USB port&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 07:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1832690#M25120</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2024-03-21T07:34:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1833517#M25129</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I'm trying to flash a new file with entering the password at the GDB server parameter and it always fails.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Ok, so you can attach with debugger after providing the password? Are you able to debug?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 07:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1833517#M25129</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-03-22T07:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1833803#M25133</link>
      <description>&lt;P&gt;No, I can't&lt;BR /&gt;I can't neither flash a new file nor start a debug session.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 14:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1833803#M25133</guid>
      <dc:creator>abdelrhman</dc:creator>
      <dc:date>2024-03-22T14:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744p censorship</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1837090#M25164</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I was talking to guys from S32DS team.&lt;/P&gt;
&lt;P&gt;There will pop up window where you enter the password. So it should be pretty simple.&lt;/P&gt;
&lt;P&gt;You dont need a script or something else like in case of Lauterbach.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 28 Mar 2024 08:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744p-censorship/m-p/1837090#M25164</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-03-28T08:09:48Z</dc:date>
    </item>
  </channel>
</rss>