<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5676R Internal Temperature Sensor in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5676R-Internal-Temperature-Sensor/m-p/489026#M2495</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;These internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual. Of course accuracy will be better than +/-10 °C as these values are corner cases.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 May 2016 08:36:10 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2016-05-02T08:36:10Z</dc:date>
    <item>
      <title>MPC5676R Internal Temperature Sensor</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5676R-Internal-Temperature-Sensor/m-p/489025#M2494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The datasheet for this device states that the accuracy is +/- 10 degrees Celsius. Is this true if the internal calibration constants are used or can you obtain a better accuracy when using the internal calibration parameters?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 16:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5676R-Internal-Temperature-Sensor/m-p/489025#M2494</guid>
      <dc:creator>nicklabianco</dc:creator>
      <dc:date>2016-04-29T16:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5676R Internal Temperature Sensor</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5676R-Internal-Temperature-Sensor/m-p/489026#M2495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;These internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual. Of course accuracy will be better than +/-10 °C as these values are corner cases.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 08:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5676R-Internal-Temperature-Sensor/m-p/489026#M2495</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-05-02T08:36:10Z</dc:date>
    </item>
  </channel>
</rss>