<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CSE Interrupt enable not working in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1811020#M24909</link>
    <description>&lt;P&gt;If SRR0 really points to this command then the problem is not caused by interrupt but rather directly by store instruction.&lt;/P&gt;
&lt;P&gt;To make it faster - is it possible to share some simplified project, so I can check it on my side?&lt;/P&gt;
&lt;P&gt;Or maybe elf file could be sufficient - in this case, I&amp;nbsp; just need to know an address of this command. And, if possible, make sure that I can reach this command independently of your system (like call it somewhere at the beginning of main function...).&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Mon, 19 Feb 2024 15:15:10 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-02-19T15:15:10Z</dc:date>
    <item>
      <title>CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1808997#M24897</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was trying to enable the interrupt for the CSE but anytime i try that my code jumps to IVOR3 and the strange part is that all the IRQq work fine except the IRQ for CSE which makes the sw jump to exception&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 09:43:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1808997#M24897</guid>
      <dc:creator>Othmane1</dc:creator>
      <dc:date>2024-02-15T09:43:49Z</dc:date>
    </item>
    <item>
      <title>Re: CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1809782#M24901</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210634"&gt;@Othmane1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let's start from the beginning - which device do you have? Which SW drivers? &lt;BR /&gt;Did you check if the vector table contains correct interrupt vector? Can you see the interrupt handlet at that address? If you put a breakpoint at the first instruction of the handler, can you reach that breakpoint? &lt;BR /&gt;When you reach the IVOR3, what is the content of core register SRR0? This should show "Set to the effective address of the excepting instruction".&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 07:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1809782#M24901</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-16T07:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1809940#M24902</link>
      <description>&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;which device do you have? &lt;STRONG&gt;Evaluation board for MPC5777C&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which SW drivers? &lt;STRONG&gt;cse_driver.c&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Did you check if the vector table contains correct interrupt vector? &lt;STRONG&gt;Yes&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can you see the interrupt handlet at that address? If you put a breakpoint at the first instruction of the handler, can you reach that breakpoint? &lt;STRONG&gt;No because the problem in eabling the interrupt whenever i try to enable that one the sw immediately&amp;nbsp;go to IVOR3&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Othmane1_0-1708084205150.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263486iDE2735DD76D5E1CA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Othmane1_0-1708084205150.png" alt="Othmane1_0-1708084205150.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 11:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1809940#M24902</guid>
      <dc:creator>Othmane1</dc:creator>
      <dc:date>2024-02-16T11:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1810619#M24907</link>
      <description>&lt;P&gt;What about the core register SRR0? This should help to understand from which address the core tries to fetch a code.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 06:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1810619#M24907</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-19T06:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1810625#M24908</link>
      <description>&lt;P&gt;IT gives me the address of this instruction:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Othmane1_0-1708325643356.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263645i69BC2C8F36189025/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Othmane1_0-1708325643356.png" alt="Othmane1_0-1708325643356.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 06:54:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1810625#M24908</guid>
      <dc:creator>Othmane1</dc:creator>
      <dc:date>2024-02-19T06:54:13Z</dc:date>
    </item>
    <item>
      <title>Re: CSE Interrupt enable not working</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1811020#M24909</link>
      <description>&lt;P&gt;If SRR0 really points to this command then the problem is not caused by interrupt but rather directly by store instruction.&lt;/P&gt;
&lt;P&gt;To make it faster - is it possible to share some simplified project, so I can check it on my side?&lt;/P&gt;
&lt;P&gt;Or maybe elf file could be sufficient - in this case, I&amp;nbsp; just need to know an address of this command. And, if possible, make sure that I can reach this command independently of your system (like call it somewhere at the beginning of main function...).&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 15:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CSE-Interrupt-enable-not-working/m-p/1811020#M24909</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-19T15:15:10Z</dc:date>
    </item>
  </channel>
</rss>