<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックUsing CAN communication with board MPC5744P</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1805227#M24877</link>
    <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;When communicating over CAN bus using MPC5744P and DEVKIT-MOTORGD, is there a specific change in jumpers positions to enable this or not? Please, show me the right positions of jumpers to achieve this. And also, is it a must to supply the board externally by 12 V when using CAN module or can I still supply it from USB as normal?&lt;/P&gt;&lt;P&gt;Thank you in advance.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 12 Feb 2024 12:27:33 GMT</pubDate>
    <dc:creator>Ahmed_Abd_El-Hafez</dc:creator>
    <dc:date>2024-02-12T12:27:33Z</dc:date>
    <item>
      <title>Using CAN communication with board MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1805227#M24877</link>
      <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;When communicating over CAN bus using MPC5744P and DEVKIT-MOTORGD, is there a specific change in jumpers positions to enable this or not? Please, show me the right positions of jumpers to achieve this. And also, is it a must to supply the board externally by 12 V when using CAN module or can I still supply it from USB as normal?&lt;/P&gt;&lt;P&gt;Thank you in advance.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 12:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1805227#M24877</guid>
      <dc:creator>Ahmed_Abd_El-Hafez</dc:creator>
      <dc:date>2024-02-12T12:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: Using CAN communication with board MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1805288#M24878</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could you please specify the DEVKIT-MPC5744P revision you have so we can suggest jumper setting?&lt;BR /&gt;Anyway with&amp;nbsp;&lt;SPAN&gt;DEVKIT-MOTORGD connected&amp;nbsp;you should configure&amp;nbsp;DEVKIT-MPC5744P to be powered&amp;nbsp;from external supply, refer to&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-devkit-motorgd:NGS-DEVKIT-MOTORGD?section=build-the-setup" target="_blank"&gt;https://www.nxp.com/document/guide/getting-started-with-the-devkit-motorgd:NGS-DEVKIT-MOTORGD?section=build-the-setup&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 14:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1805288#M24878</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-12T14:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: Using CAN communication with board MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1806414#M24893</link>
      <description>&lt;P&gt;thank you for your response. First thing ,My board is REV E . secondly, I did not know that I should configure the MPC5744P to be externally supplied. I supplied it by usb from my laptop&amp;nbsp; and supplied the Devkit-Motor GD by the 12 V and it works and the motor runs. what is the difference or why should I supply it externaly? or it is necessary with communicating over CAN module only.&lt;/P&gt;&lt;P&gt;also I need to know the jumpers position for enabling communicating over CAN module if any.&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 09:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1806414#M24893</guid>
      <dc:creator>Ahmed_Abd_El-Hafez</dc:creator>
      <dc:date>2024-02-14T09:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: Using CAN communication with board MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1809045#M24898</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;at least it is mentioned in&amp;nbsp;&lt;SPAN&gt;DEVKIT-MOTORGD getting started&amp;nbsp;&lt;/SPAN&gt;guide, I mentioned. In that case&amp;nbsp;&lt;SPAN&gt;DEVKIT-MPC5744P will use power delivered from&amp;nbsp;DEVKIT-MOTORGD and single supply will be used.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;On DEVKIT-MPC5744P rev.E CAN transceiver is integrated in SBC, and thus external 12V must be used to power&amp;nbsp;DEVKIT-MPC5744P.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Can be done using board's power jack or if taken from plugged&amp;nbsp;DEVKIT-MOTORGD, in that case J39 should be installed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;CAN TXD/RXD signals are selected using J174. by default FlexCAN0 on pins PTB0/PTB1 is connected to SBC CAN transceiver.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 10:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Using-CAN-communication-with-board-MPC5744P/m-p/1809045#M24898</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-15T10:57:37Z</dc:date>
    </item>
  </channel>
</rss>