<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: STANDBY mode entry problem in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/STANDBY-mode-entry-problem/m-p/1802672#M24853</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;usually what prevents entering the STANDBY is active clock on some peripheral. For example CAN, PWM, etc... As this clock will not be aviable in STANDBY it is recommended to deactivate it first and then do mode transition.&lt;/P&gt;
&lt;P&gt;Just a blind shot.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Tue, 06 Feb 2024 12:50:49 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2024-02-06T12:50:49Z</dc:date>
    <item>
      <title>STANDBY mode entry problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/STANDBY-mode-entry-problem/m-p/1802478#M24848</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have problem with entering STANDBY mode at MPC5606B.&lt;BR /&gt;I use following code to switch between modes. Transition into STOP mode or RUNx modes works fine, but when I want to go to STANDBY mode, ME_GS.MTRANS bit is set to 1 (transition ongoing) and never resets to 0.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;int halSPCSetRunMode(spc5_runmode_t mode)
{
  /* Starts a transition process.*/
  ME.MCTL.R = SPC5_ME_MCTL_MODE(mode) | SPC5_ME_MCTL_KEY;
  ME.MCTL.R = SPC5_ME_MCTL_MODE(mode) | SPC5_ME_MCTL_KEY_INV;

  while (true) {
    uint32_t r = ME.GS.B.MTRANS;
    if (r == 0) {
        return 1;
    }
  }
}&lt;/LI-CODE&gt;&lt;P&gt;I have no idea what to look at or what could be the problem. I would be grateful for any help.&lt;/P&gt;&lt;P&gt;Thank you beforehand.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 08:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/STANDBY-mode-entry-problem/m-p/1802478#M24848</guid>
      <dc:creator>snafu</dc:creator>
      <dc:date>2024-02-06T08:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: STANDBY mode entry problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/STANDBY-mode-entry-problem/m-p/1802672#M24853</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;usually what prevents entering the STANDBY is active clock on some peripheral. For example CAN, PWM, etc... As this clock will not be aviable in STANDBY it is recommended to deactivate it first and then do mode transition.&lt;/P&gt;
&lt;P&gt;Just a blind shot.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 12:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/STANDBY-mode-entry-problem/m-p/1802672#M24853</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-02-06T12:50:49Z</dc:date>
    </item>
  </channel>
</rss>