<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5748G ENET</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488470#M2472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/tomyqg"&gt;tomyqg&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lukaszadrapa"&gt;lukaszadrapa&lt;/A&gt;​ mentioned in this thread &lt;A href="https://community.nxp.com/message/818142"&gt;mpc5748g enet d-cache&lt;/A&gt; you have to configure the SMPU (System Memory Protection Unit) according to the example. To only have the Rx and Tx descriptors non cachable I defined a section in Project_Settings/Linker_Files/sections.ld&amp;nbsp; at the text section with this content:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* area excluded from d-cache and i-cache via smpu */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .non_cache (NOLOAD) : ALIGN(64)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __NON_CACHE_START = .;&lt;/P&gt;&lt;P&gt;&amp;nbsp; *(.lwip_descriptors);&lt;/P&gt;&lt;P&gt;&amp;nbsp; __NON_CACHE_END = .;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&amp;nbsp; &amp;gt; m_data AT&amp;gt;m_text&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I told the linker to put the descriptors to this section (in eth.c):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;__attribute__(( aligned(64), section(".lwip_descriptors") ))&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally the SMPU must be configured to prevent caching at this section (this is mostly copied from the example):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;extern char __NON_CACHE_START;&amp;nbsp; // sourced from Project_Settings/Startup_Code/sections.ld&lt;/P&gt;&lt;P&gt;extern char __NON_CACHE_END; // sourced fromProject_Settings/Startup_Code/sections.ld&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void smpu_config(void) {&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Ensure SMPU modules are disabled */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_0.CES0.B.GVLD = 0;&amp;nbsp;&amp;nbsp; /* Allow all accesses from all masters to SMPU0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.CES0.B.GVLD = 0;&amp;nbsp;&amp;nbsp; /* Allow all accesses from all masters to SMPU1 */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Create desired memory regions */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Region 0:&amp;nbsp; From __NON_CACHE_START to __NON_CACHE_STOP disable caching&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; this is from the beginning of RAM to __NON_CACHE_STOP */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD0.R = (uint32_t)&amp;amp;__NON_CACHE_START;&amp;nbsp; /* Region start addr- start of SRAM */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD1.R = (uint32_t)&amp;amp;__NON_CACHE_END;&amp;nbsp; /* Region end addr- end of SRAM&amp;nbsp; */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD2.FMT0.R = 0xFFFFFFFF; /* ALL masters can read/write */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD3.R = 0x00000002;&amp;nbsp; /* Region non-cacheable: Cache Inhibit=2*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD4.R = 0x00000000;&amp;nbsp; /* PID not included in region eval. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[0].WORD5.R = 0x00000001;&amp;nbsp; /* Region is valid without lock */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Region 1:&amp;nbsp; enable caching for the rest of RAM */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD0.R = (uint32_t)&amp;amp;__NON_CACHE_END; /* Reg start addr*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD1.R = 0x400BFFFF; /*Region end */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD2.FMT0.R = 0xFFFFFFFF; /* ALL masters can read/write */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD3.R = 0x00000000;&amp;nbsp; /* Region cacheable: Cache Inhibit=0*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD4.R = 0x00000000;&amp;nbsp; /* PID not included in region eval. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.RGD[1].WORD5.R = 0x00000001;&amp;nbsp; /* Region is valid without lock */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable all SMPU regions in module */&lt;/P&gt;&lt;P&gt;/*&amp;nbsp; SMPU_0.CES0.B.GVLD = 1;*/ /* -- NOT USED IN CODE EXAMPLE --SMPU0&amp;nbsp; */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMPU_1.CES0.B.GVLD = 1;&amp;nbsp;&amp;nbsp; /* SMPU1 is enabled */&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Aug 2016 16:23:08 GMT</pubDate>
    <dc:creator>bdn</dc:creator>
    <dc:date>2016-08-03T16:23:08Z</dc:date>
    <item>
      <title>MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488434#M2436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! Is there any examples or documents where I can find information on how to configure and use ENET on MPC5748G?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 10:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488434#M2436</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-02-25T10:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488435#M2437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have ENET driver for MPC5775K, but it should be the same module as on the MPC5748G. Maybe it will be necessary to update some register names because of different header files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Feb 2016 06:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488435#M2437</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-02-29T06:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488436#M2438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! Thank you for the examle code. I will try to make it work =)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Feb 2016 07:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488436#M2438</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-02-29T07:26:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488437#M2439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Still no luck getting the ENET to work. Do i need to do something with the switch that 5748 uses?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 13:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488437#M2439</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-03-02T13:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488438#M2440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please more clarify your problem? Are you able to build/compile the project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 07:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488438#M2440</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-03-03T07:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488439#M2441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My task is to send an ethernet packet from my eval board to my computer. The project can build/compile without errors. Im using the example code you gave me with some changes to the GPIO init function. As now I am using Wireshark to capture packets sendt on the network. If I understand correctly the buffer is sent when TDAR is 1 and I should be able to see the packet on the network, right ? As long as my GPIO is initialized correctly. However, after TDAR is set, there is nothing to caputre from 5748G. I think the problem is my setup of the gpio, or the clock maby. Is there anyway to debug the transmission of the buffer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2016 11:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488439#M2441</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-03-04T11:14:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488440#M2442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;at first, try to measure signal on Tx pin, if you are able to transmit something. You are correct about TDAR, but wireshark is able to display only PDU, which has correct format.&amp;nbsp; So wireshark is the last possibility to debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 12:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488440#M2442</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-03-07T12:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488441#M2443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is a good point. Gotta freshen up some skills with the scope then. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 14:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488441#M2443</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-03-09T14:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488442#M2444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am also working on the Ethernet for MPC5748G. I am also having same trouble. &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sondre89"&gt;sondre89&lt;/A&gt; did you successfully run the ENET program. If yes please can you share the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 19:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488442#M2444</guid>
      <dc:creator>kushalshah</dc:creator>
      <dc:date>2016-03-11T19:00:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488443#M2445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! Im currently working with something else right now, so i have not been able to complete my ethernet code. However, I have confirmed that the example code, with some changes to the gpio's to fit 5748G, is able to transmit data out of the processor to the ethernet controller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 07:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488443#M2445</guid>
      <dc:creator>sondre89</dc:creator>
      <dc:date>2016-03-14T07:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488444#M2446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sondre89"&gt;sondre89&lt;/A&gt; for the reply. I was able to run the Ethernet program after changing GPIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 12:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488444#M2446</guid>
      <dc:creator>kushalshah</dc:creator>
      <dc:date>2016-03-14T12:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488445#M2447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Kushal Shah! I am also working on the Ethernet for MPC5748G, but i don't know what i need to change in the example code&amp;nbsp; to run the Ethernet program correctly. &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;if it's possible, p&lt;/SPAN&gt;&lt;/SPAN&gt;lease can you share your project code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alex.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 16:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488445#M2447</guid>
      <dc:creator>alextimpau</dc:creator>
      <dc:date>2016-03-14T16:24:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488446#M2448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/alextimpau"&gt;alextimpau&lt;/A&gt;​, here is the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is targeted to NXP X-MPC574xG-Mother board and Daughter card board. And this project is made using S32 Design Studio for Power.&lt;/P&gt;&lt;P&gt;It will toggle LED DS2 when it receives the data.&lt;/P&gt;&lt;P&gt;You can use Packet Sender app for this.&lt;/P&gt;&lt;P&gt;Finally it sends packets using UDP protocol.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 18:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488446#M2448</guid>
      <dc:creator>kushalshah</dc:creator>
      <dc:date>2016-03-14T18:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488447#M2449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="238960" data-username="kushalshah" href="https://community.nxp.com/people/kushalshah"&gt;Kushal Shah!&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you very much! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt; Alex.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 18:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488447#M2449</guid>
      <dc:creator>alextimpau</dc:creator>
      <dc:date>2016-03-14T18:36:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488448#M2450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kushal Shah!&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I have a problem when trying to upload the &lt;SPAN&gt;source&lt;/SPAN&gt; &lt;SPAN&gt;code: &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="short_text" lang="en"&gt;in the final stage of debugging this &lt;SPAN&gt;error occurred&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV dir="ltr"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="error.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/23433i31E06742A4AF514E/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.png" alt="error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt;&lt;SPAN class="ita-kd-inputtools-div"&gt;&lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P class="almost_half_cell"&gt;&lt;SPAN lang="en"&gt;Could you please tell me what changes should I do to run this application successfully&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="almost_half_cell"&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alex.&lt;/P&gt;&lt;DIV dir="ltr"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Mar 2016 15:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488448#M2450</guid>
      <dc:creator>alextimpau</dc:creator>
      <dc:date>2016-03-20T15:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488449#M2451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is the problem of S32DS. Look at these following threads. We have already solved this problem, so there are some points which you can try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/386262"&gt;I have an error : Launching  L1_Z4.elf has encoutered a problem.Error starting process. &lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/386055"&gt;P&amp;amp;amp;E Connection Assistant Error &lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Mar 2016 06:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488449#M2451</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-03-21T06:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488450#M2452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/kushalshah13"&gt;kushalshah13&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your example project.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I am also working on the Ethernet for MPC5748G. I have the &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;X-MPC574xG-Mother board and Daughter card board.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Can you tell me how to you test the project whether it works right?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Did you recrive packet by Wireshark?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;And can you tell me which &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Packet Sender app can be helpful?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thank you very much!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Qiang&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Mar 2016 08:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488450#M2452</guid>
      <dc:creator>huqiang</dc:creator>
      <dc:date>2016-03-26T08:10:48Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488451#M2453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/huqiang"&gt;huqiang&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use wire-shark to observe the received packets.&lt;/P&gt;&lt;P&gt;The name of other app is itself is "Packet-sender"( &lt;A href="https://packetsender.com/"&gt;https://packetsender.com/&lt;/A&gt;​)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The project is configured in polling mode for transferring packets and in the interrupt mode for receiving packets. Watch for transferred packet in above two apps directly. And for received packets interrupt is generated which toggles the DS2 LED on mother board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kushal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Mar 2016 14:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488451#M2453</guid>
      <dc:creator>kushalshah</dc:creator>
      <dc:date>2016-03-28T14:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488452#M2454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/kushalshah"&gt;kushalshah&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;Thank you for your suggestion.&lt;/P&gt;&lt;P&gt;I will try it later.&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Regards,&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Qiang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Mar 2016 15:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488452#M2454</guid>
      <dc:creator>huqiang</dc:creator>
      <dc:date>2016-03-28T15:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G ENET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488453#M2455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have ported LWIP into MPC5748G project which used simple ethernet drivers including initialization, send package and receive package. Maybe you can have a reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neil Li(李越)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 08:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-ENET/m-p/488453#M2455</guid>
      <dc:creator>yueli</dc:creator>
      <dc:date>2016-03-30T08:00:14Z</dc:date>
    </item>
  </channel>
</rss>