<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32DS IDE code issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/S32DS-IDE-code-issue/m-p/1744770#M24439</link>
    <description>&lt;P&gt;A customer of mine reported a crash in their application. After some investigation I think the problem is coming from some instruction errors as shown in the S32DS IDE file NXP/BSP/Startup/MPC5748G/gnu/interrupt_vectors.S in IVOR4X_Handler, the code snip is:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;e_lis r11,OS_CPU_ISRNestingCtr@ha # Increment the ISR nesting counter to reflect the current nesting level.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_or2i r11,OS_CPU_ISRNestingCtr@l # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_lwz r12,0(r11) # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_add2i. r12,1 # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_stw r12,0(r11) # ...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;It seems e_lis with the &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155811"&gt;@ha&lt;/a&gt; notation followed by e_or2i with the @l notation is wrong. A possible solution is to use the @h notation in the first instruction (e_lis r11,OS_CPU_ISRNestingCtr@ha ). I noticed the error is repeated in IntStkInUse and OSIntCtxSw. I did not search other files for similar problems.&lt;/P&gt;</description>
    <pubDate>Mon, 23 Oct 2023 20:49:30 GMT</pubDate>
    <dc:creator>Traci</dc:creator>
    <dc:date>2023-10-23T20:49:30Z</dc:date>
    <item>
      <title>S32DS IDE code issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32DS-IDE-code-issue/m-p/1744770#M24439</link>
      <description>&lt;P&gt;A customer of mine reported a crash in their application. After some investigation I think the problem is coming from some instruction errors as shown in the S32DS IDE file NXP/BSP/Startup/MPC5748G/gnu/interrupt_vectors.S in IVOR4X_Handler, the code snip is:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;e_lis r11,OS_CPU_ISRNestingCtr@ha # Increment the ISR nesting counter to reflect the current nesting level.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_or2i r11,OS_CPU_ISRNestingCtr@l # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_lwz r12,0(r11) # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_add2i. r12,1 # ...&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;e_stw r12,0(r11) # ...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;It seems e_lis with the &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155811"&gt;@ha&lt;/a&gt; notation followed by e_or2i with the @l notation is wrong. A possible solution is to use the @h notation in the first instruction (e_lis r11,OS_CPU_ISRNestingCtr@ha ). I noticed the error is repeated in IntStkInUse and OSIntCtxSw. I did not search other files for similar problems.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Oct 2023 20:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32DS-IDE-code-issue/m-p/1744770#M24439</guid>
      <dc:creator>Traci</dc:creator>
      <dc:date>2023-10-23T20:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS IDE code issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32DS-IDE-code-issue/m-p/1745058#M24441</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215856"&gt;@Traci&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes, you are right. It was already discussed here, for example:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/e-lis-problem-for-S32R274-Z7a-Core/m-p/1262524/highlight/true#M17986" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/e-lis-problem-for-S32R274-Z7a-Core/m-p/1262524/highlight/true#M17986&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 07:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32DS-IDE-code-issue/m-p/1745058#M24441</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-10-24T07:06:41Z</dc:date>
    </item>
  </channel>
</rss>