<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 EXTCLK MPC561</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EXTCLK-MPC561/m-p/1689107#M23959</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use a MPC561 with a problem of startup.&lt;/P&gt;&lt;P&gt;The EXTCLK and JCOMP signals are not connected.&lt;/P&gt;&lt;P&gt;Can these unconnected signals generate a problem of startup ?&lt;/P&gt;&lt;P&gt;Thank you in advanced&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jul 2023 07:29:54 GMT</pubDate>
    <dc:creator>christophe_c</dc:creator>
    <dc:date>2023-07-20T07:29:54Z</dc:date>
    <item>
      <title>EXTCLK MPC561</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EXTCLK-MPC561/m-p/1689107#M23959</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use a MPC561 with a problem of startup.&lt;/P&gt;&lt;P&gt;The EXTCLK and JCOMP signals are not connected.&lt;/P&gt;&lt;P&gt;Can these unconnected signals generate a problem of startup ?&lt;/P&gt;&lt;P&gt;Thank you in advanced&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 07:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EXTCLK-MPC561/m-p/1689107#M23959</guid>
      <dc:creator>christophe_c</dc:creator>
      <dc:date>2023-07-20T07:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: EXTCLK MPC561</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EXTCLK-MPC561/m-p/1689436#M23961</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/148297"&gt;@christophe_c&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there should be no problem with unconnected JCOMP. It is internally pulled down which enables BDM/Nexus pins instead of JTAG.&lt;/P&gt;
&lt;P&gt;But unconnected EXTCLK could be an issue - if it is not used, it must be tied to GND.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 13:02:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EXTCLK-MPC561/m-p/1689436#M23961</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-07-20T13:02:22Z</dc:date>
    </item>
  </channel>
</rss>