<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Dcache as RAM to increase RAM size in MPC5777C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-to-increase-RAM-size-in-MPC5777C/m-p/1659272#M23726</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi everyone, I want to&amp;nbsp; use dcache as ram to increase the available ram size. I referred a cookbook (AN2865&amp;nbsp;Qorivva Simple Cookbook) in the section Cache as RAM it says, to use cache as ram the cache should be invalidated and enabled in copyback mode. All I want is to increase my ram size my using &lt;STRONG&gt;dcache 16kb memory as ram&lt;/STRONG&gt; is that possible is possible how?&lt;BR /&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Indra&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 29 May 2023 17:57:19 GMT</pubDate>
    <dc:creator>Indra</dc:creator>
    <dc:date>2023-05-29T17:57:19Z</dc:date>
    <item>
      <title>Dcache as RAM to increase RAM size in MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-to-increase-RAM-size-in-MPC5777C/m-p/1659272#M23726</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi everyone, I want to&amp;nbsp; use dcache as ram to increase the available ram size. I referred a cookbook (AN2865&amp;nbsp;Qorivva Simple Cookbook) in the section Cache as RAM it says, to use cache as ram the cache should be invalidated and enabled in copyback mode. All I want is to increase my ram size my using &lt;STRONG&gt;dcache 16kb memory as ram&lt;/STRONG&gt; is that possible is possible how?&lt;BR /&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Indra&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 29 May 2023 17:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-to-increase-RAM-size-in-MPC5777C/m-p/1659272#M23726</guid>
      <dc:creator>Indra</dc:creator>
      <dc:date>2023-05-29T17:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: Dcache as RAM to increase RAM size in MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-to-increase-RAM-size-in-MPC5777C/m-p/1660895#M23740</link>
      <description>&lt;P&gt;It is the same thread as following:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-in-MPC5777C/m-p/1660816/highlight/false#M23737" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-in-MPC5777C/m-p/1660816/highlight/false#M23737&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 14:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-to-increase-RAM-size-in-MPC5777C/m-p/1660895#M23740</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-05-31T14:44:41Z</dc:date>
    </item>
  </channel>
</rss>