<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Program flash startup failed in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1629126#M23318</link>
    <description>&lt;P&gt;Hi,&lt;SPAN&gt;Peter:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sorry, the problem description was not very clear. What I would like to inquire about is that in the [MPC574XG'_ MCAL4_ 0_ RTM_ 1_ 0_ 5_ Sample_ Application], I see [FLASH_START] in the file [flashrchw. c], so I would like to use GHS to compile the OS project of MPC5748G with [FLASH_START]. May I ask what command or method should be used to compile the project of [FLASH_START]. Additionally, what else should be noted when compiling such a project.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Apr 2023 12:49:16 GMT</pubDate>
    <dc:creator>wangjain</dc:creator>
    <dc:date>2023-04-06T12:49:16Z</dc:date>
    <item>
      <title>Program flash startup failed</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1628281#M23313</link>
      <description>&lt;P&gt;I am using devkit mpc5748g and 'MPC574XG'_ MCAL4_ 0_ RTM_ 1_ 0_ 5_ Sample_ Application 'sample program, compiled using GHS for toolchain. Use the command '/ launch.bat OS TOOLCHAIN=ghs&lt;/P&gt;&lt;P&gt;’Compile the program and pass the compilation. Next, use S32DS for flash download of the code, and after successful download, the program runs normally. However, when I unplugged the power and turned it on again, I found that the running program was inconsistent with the program before the power outage. May I ask how to solve this problem? Thank you very much.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 13:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1628281#M23313</guid>
      <dc:creator>wangjain</dc:creator>
      <dc:date>2023-04-05T13:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash startup failed</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1628712#M23315</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;after successful download, the program runs normally. However, when I unplugged the power and turned it on again, I found that the running program was inconsistent with the program before the power outage.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Since power outage does not affect flash content I expect there is RAM init issue. As RAM loose content after power on reset.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;program was inconsistent with the program before&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Could you specify what was inconsistent? Memory content?&lt;/P&gt;
&lt;P&gt;Could you share more detailed failure analyzes details?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 04:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1628712#M23315</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-04-06T04:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash startup failed</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1629126#M23318</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;Peter:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sorry, the problem description was not very clear. What I would like to inquire about is that in the [MPC574XG'_ MCAL4_ 0_ RTM_ 1_ 0_ 5_ Sample_ Application], I see [FLASH_START] in the file [flashrchw. c], so I would like to use GHS to compile the OS project of MPC5748G with [FLASH_START]. May I ask what command or method should be used to compile the project of [FLASH_START]. Additionally, what else should be noted when compiling such a project.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 12:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1629126#M23318</guid>
      <dc:creator>wangjain</dc:creator>
      <dc:date>2023-04-06T12:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash startup failed</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1630999#M23340</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I am not clear what you want to achieve. Do you have experience with AUTOSAR and its configuration tools already?&lt;/P&gt;
&lt;P&gt;Because that is essential to be able understand and build any example.&lt;/P&gt;
&lt;P&gt;I see you are referring to MCAL and now to OS (which one?)&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;[FLASH_START] in the file [flashrchw. c]&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;This looks like a part of S32DS for core control. So you are using GHS compiler plugin in S32DS right?&lt;/P&gt;
&lt;P&gt;Unfortunately from your brief explanation I am not able to understand what is your setup and what you want to achieve.&lt;/P&gt;
&lt;P&gt;What could help you in orientation is our HOW TOs for S32DS:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 06:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Program-flash-startup-failed/m-p/1630999#M23340</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-04-11T06:37:29Z</dc:date>
    </item>
  </channel>
</rss>