<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMPC5784G Core2 Not Working without RESET</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615708#M23178</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MPC5748G Controller, where I am using Core 2 for programming TFT Display, the problem I am facing is display does not come up until I RESET the Microcontroller using the SW1 on the hardware, but core 1 will work without RESET as soon as powered up. Please suggest if there is any solution for this.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 15 Mar 2023 12:28:01 GMT</pubDate>
    <dc:creator>Charith</dc:creator>
    <dc:date>2023-03-15T12:28:01Z</dc:date>
    <item>
      <title>MPC5784G Core2 Not Working without RESET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615708#M23178</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MPC5748G Controller, where I am using Core 2 for programming TFT Display, the problem I am facing is display does not come up until I RESET the Microcontroller using the SW1 on the hardware, but core 1 will work without RESET as soon as powered up. Please suggest if there is any solution for this.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 15 Mar 2023 12:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615708#M23178</guid>
      <dc:creator>Charith</dc:creator>
      <dc:date>2023-03-15T12:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5784G Core2 Not Working without RESET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615799#M23180</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you please share how do you start core2?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 15 Mar 2023 13:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615799#M23180</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-03-15T13:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5784G Core2 Not Working without RESET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615832#M23184</link>
      <description>Should I send Startup Code.</description>
      <pubDate>Wed, 15 Mar 2023 14:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1615832#M23184</guid>
      <dc:creator>Charith</dc:creator>
      <dc:date>2023-03-15T14:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5784G Core2 Not Working without RESET</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1616596#M23200</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Well that wont be necessary. I am interested only on how do you start core2.&lt;/P&gt;&lt;P&gt;Below is the example how it should looks like, as you see, no reset is needed. In fact reset will put core2 into reset state.&lt;/P&gt;&lt;P&gt;What you are describing is not possible to achieve from HW standpoint concept of this micro.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;void Core_Boot (void)&lt;BR /&gt;{&lt;BR /&gt;/* ~~~~~~~~~~~~~~~~~~~~~~~ Configure Cores ~~~~~~~~~~~~~~~~~~~~~~~~~ */ &lt;BR /&gt;/* Enable Cores - Will start on next mode transistion */&lt;BR /&gt;&lt;BR /&gt;//MC_ME.CCTL1.R = 0x00FE; // (z4a) - boot core_0 is active&lt;BR /&gt;MC_ME.CCTL[2].R = 0x00FE; // (z4b) - core_1 is active&lt;BR /&gt;MC_ME.CCTL[3].R = 0x00FE; // (z2) - core_2 is active&lt;BR /&gt;&lt;BR /&gt;/* Set Start address for other cores: Will reset and start */&lt;BR /&gt;/* Flash addresses */&lt;BR /&gt;MC_ME.CADDR[2].R = 0x00F90001; // core_1 (z4b) boot address&lt;BR /&gt;MC_ME.CADDR[3].R = 0x00F9C001; // core_2 (z2) boot address&lt;BR /&gt;&lt;BR /&gt;/****************************** Preform mode change **************************/&lt;BR /&gt;&lt;BR /&gt;/* Mode change Re-enter the drun mode, to start cores */&lt;BR /&gt;MC_ME.MCTL.R = 0x30005AF0; /* Mode &amp;amp; Key */&lt;BR /&gt;MC_ME.MCTL.R = 0x3000A50F; /* Mode &amp;amp; Key inverted */&lt;BR /&gt;&lt;BR /&gt;while(MC_ME.GS.B.S_MTRANS == 1); /* Wait for mode entry complete */&lt;BR /&gt;while(MC_ME.GS.B.S_CURRENT_MODE != 0x3); /* Check DRUN mode entered */&lt;BR /&gt;&lt;BR /&gt;}//Core_Boot&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 09:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5784G-Core2-Not-Working-without-RESET/m-p/1616596#M23200</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-03-16T09:17:38Z</dc:date>
    </item>
  </channel>
</rss>