<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN Message RAM configuration in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610841#M23055</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213706"&gt;@Noobie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there's 9.5KB RAM only as mentioned in section 41.1.1.&lt;/P&gt;
&lt;P&gt;The address range 0xFFE3_4000–0xFFE3_7FFF does not say that there's exactly the same amount of RAM. This range is used due to alignment.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Tue, 07 Mar 2023 10:51:43 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2023-03-07T10:51:43Z</dc:date>
    <item>
      <title>CAN Message RAM configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610031#M23037</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I'm using MPC5777C controller.&lt;BR /&gt;&lt;BR /&gt;In the data-sheet of the controller under memory map section, it is mentioned that M_CAN RAM is from 0xFFE3_4000 to 0xFFE3_7FFF. This I believe to be of 15.99KB.&lt;BR /&gt;&lt;BR /&gt;But, under chip-specific M_CAN information it is mentioned that Message RAM supports 9.5KB.&lt;BR /&gt;&lt;BR /&gt;May I know if M_CAN will support 15.99KB RAM or 9.5 KB ?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Mar 2023 13:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610031#M23037</guid>
      <dc:creator>Noobie</dc:creator>
      <dc:date>2023-03-06T13:14:13Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Message RAM configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610841#M23055</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213706"&gt;@Noobie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there's 9.5KB RAM only as mentioned in section 41.1.1.&lt;/P&gt;
&lt;P&gt;The address range 0xFFE3_4000–0xFFE3_7FFF does not say that there's exactly the same amount of RAM. This range is used due to alignment.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 10:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610841#M23055</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-03-07T10:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Message RAM configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610875#M23057</link>
      <description>&lt;P&gt;Hello Lukas,&lt;BR /&gt;&lt;BR /&gt;Thank you for the response.&lt;BR /&gt;&lt;BR /&gt;Regards.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 12:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-Message-RAM-configuration/m-p/1610875#M23057</guid>
      <dc:creator>Noobie</dc:creator>
      <dc:date>2023-03-07T12:06:15Z</dc:date>
    </item>
  </channel>
</rss>