<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Microcontroller-MPC5675K-Reset issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1608881#M23005</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;Warm Greetings.&lt;/P&gt;&lt;P&gt;We are using SPC5675KFF0VMS2-Micro Controller for our application. We face the reset issue in the controller. Every power ON, we read the status of the Functional (RGM_FES)as well as Destructive event status register(RGM_DES). (Refer 46.3.1.1 in MPC5675KRM reference manual for register details)&lt;/P&gt;&lt;P&gt;It was updated as,&lt;/P&gt;&lt;P&gt;Functional event status register : 0x9000&lt;/P&gt;&lt;P&gt;Destructive event status register: 0x8000&lt;/P&gt;&lt;P&gt;Even though we are resetting the controller externally after power on , the RGM_DES status remains 0x8000.&lt;/P&gt;&lt;P&gt;We followed following sequence,&lt;/P&gt;&lt;P&gt;1) Read the RGM_FES &amp;amp; RGM_DES register after power ON&lt;/P&gt;&lt;P&gt;2) Clearing the status register and read back the same.(RGM_FES: 0x0; RGM_DES: 0x0)&lt;/P&gt;&lt;P&gt;3) After the external reset ( toggling the reset pin externally) released , the RGM_DES register should be 0x0(since POR is not happened). But it was updated as 0x8000.&lt;/P&gt;&lt;P&gt;Please provide suggestion to proceed further.&lt;/P&gt;</description>
    <pubDate>Fri, 03 Mar 2023 04:22:50 GMT</pubDate>
    <dc:creator>ArunaNellaiappan</dc:creator>
    <dc:date>2023-03-03T04:22:50Z</dc:date>
    <item>
      <title>Microcontroller-MPC5675K-Reset issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1608881#M23005</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;Warm Greetings.&lt;/P&gt;&lt;P&gt;We are using SPC5675KFF0VMS2-Micro Controller for our application. We face the reset issue in the controller. Every power ON, we read the status of the Functional (RGM_FES)as well as Destructive event status register(RGM_DES). (Refer 46.3.1.1 in MPC5675KRM reference manual for register details)&lt;/P&gt;&lt;P&gt;It was updated as,&lt;/P&gt;&lt;P&gt;Functional event status register : 0x9000&lt;/P&gt;&lt;P&gt;Destructive event status register: 0x8000&lt;/P&gt;&lt;P&gt;Even though we are resetting the controller externally after power on , the RGM_DES status remains 0x8000.&lt;/P&gt;&lt;P&gt;We followed following sequence,&lt;/P&gt;&lt;P&gt;1) Read the RGM_FES &amp;amp; RGM_DES register after power ON&lt;/P&gt;&lt;P&gt;2) Clearing the status register and read back the same.(RGM_FES: 0x0; RGM_DES: 0x0)&lt;/P&gt;&lt;P&gt;3) After the external reset ( toggling the reset pin externally) released , the RGM_DES register should be 0x0(since POR is not happened). But it was updated as 0x8000.&lt;/P&gt;&lt;P&gt;Please provide suggestion to proceed further.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 04:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1608881#M23005</guid>
      <dc:creator>ArunaNellaiappan</dc:creator>
      <dc:date>2023-03-03T04:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller-MPC5675K-Reset issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1609047#M23012</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;From your description the only possible cause is that once you trigger external reset, your also loose power to micro somehow.&lt;/P&gt;
&lt;P&gt;Please do the same with voltage monitoring via scope, to see if the power is always within datasheet specification.&lt;/P&gt;
&lt;P&gt;On top of that you can do tests on NXP Evaluation board to exclude any HW issue.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 08:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1609047#M23012</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-03-03T08:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller-MPC5675K-Reset issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1639423#M23431</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry for the delayed response.&lt;/P&gt;&lt;P&gt;As per your suggestion, We have probed the External reset as well as Microcontroller Supply line.(image attached). Though we gave the external reset,the Micro Controller didn't loose its power.&lt;/P&gt;&lt;P&gt;Provide suggestion to proceed further.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Apr 2023 05:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1639423#M23431</guid>
      <dc:creator>ArunaNellaiappan</dc:creator>
      <dc:date>2023-04-25T05:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller-MPC5675K-Reset issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1645961#M23526</link>
      <description>&lt;P&gt;The following sequence followed,&lt;/P&gt;&lt;P&gt;we cleared the power on reset bit manually by writing the 0xC3FE4002 as 1( suspecting clear is not done properly).&lt;/P&gt;&lt;P&gt;After the external reset (pin AC20) was released, the RGM_DES register remains 8000. ( Indicating power on reset happened). The queries are,&lt;/P&gt;&lt;P&gt;1) what will be the expected range of VDD_HV_xxx , VDD_LV_xxx ( during external &amp;amp; internal vreg mode)?&lt;/P&gt;&lt;P&gt;2)&amp;nbsp; how to check the&amp;nbsp; 2.7V generated inside after the reset occured?&lt;/P&gt;&lt;P&gt;3) what will be the DRAM supply voltage ?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also, Provide suggestion to proceed further&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 06 May 2023 18:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1645961#M23526</guid>
      <dc:creator>ArunaNellaiappan</dc:creator>
      <dc:date>2023-05-06T18:29:56Z</dc:date>
    </item>
    <item>
      <title>Re: Microcontroller-MPC5675K-Reset issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1646937#M23539</link>
      <description>&lt;P&gt;This is a gentle reminder.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please Provide suggestion to proceed further&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;The following sequence followed,&lt;/P&gt;&lt;P&gt;we cleared the power on reset bit manually by writing the 0xC3FE4002 as 1( suspecting clear is not done properly).&lt;/P&gt;&lt;P&gt;After the external reset (pin AC20) was released, the RGM_DES register remains 8000. ( Indicating power on reset happened). The queries are,&lt;/P&gt;&lt;P&gt;1) what will be the expected range of VDD_HV_xxx , VDD_LV_xxx ( during external &amp;amp; internal vreg mode)?&lt;/P&gt;&lt;P&gt;2)&amp;nbsp; how to check the&amp;nbsp; 2.7V generated inside after the reset occured?&lt;/P&gt;&lt;P&gt;3) what will be the DRAM supply voltage ?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 09 May 2023 08:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Microcontroller-MPC5675K-Reset-issue/m-p/1646937#M23539</guid>
      <dc:creator>ArunaNellaiappan</dc:creator>
      <dc:date>2023-05-09T08:13:59Z</dc:date>
    </item>
  </channel>
</rss>