<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5777M startup problem in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-startup-problem/m-p/1606818#M22985</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213299"&gt;@underdangerous&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;are you able to attach the debugger to running target? Please follow solution in this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Once you are attached, you can stop the execution and check what happened - if some exception was triggered etc.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Tue, 28 Feb 2023 11:49:51 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2023-02-28T11:49:51Z</dc:date>
    <item>
      <title>MPC5777M startup problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-startup-problem/m-p/1606068#M22974</link>
      <description>&lt;P&gt;Hi,everyone:&lt;/P&gt;&lt;P&gt;We now have a problem&amp;nbsp; when I connect JTAG to the target board and click Flash in file or debug in S32DS for PA v2.1,the code works correctly and the functionality is implemented as expected.But once I power off and restart the MCU, the code will not be executed,and I checked the 0x01000000 after using the NXP_MPC5777M_1x32x1984k_CFlash.pcp algorithm in PROGPPCNEXUS-Flash Programmer and found that the code had been downloaded to flash.I have already add MC_ME.PCTL15.R = 0 before the last mode, but&amp;nbsp;it didn't work.The device information is as follows：&lt;/P&gt;&lt;P&gt;Motherbroad:MPC57XXMB-REVC-SCH&lt;BR /&gt;Daughtercard:MPC5777M_512DS&lt;BR /&gt;Debugger:PEMicro USB MULTILINK UNIVERSAL&lt;/P&gt;&lt;P&gt;This problem has been bothering us for a long time,but we don't know exactly where the problem is.Hope somebody&amp;nbsp; can help us with this, thank you very much.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 12:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-startup-problem/m-p/1606068#M22974</guid>
      <dc:creator>underdangerous</dc:creator>
      <dc:date>2023-02-27T12:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M startup problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-startup-problem/m-p/1606818#M22985</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213299"&gt;@underdangerous&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;are you able to attach the debugger to running target? Please follow solution in this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Once you are attached, you can stop the execution and check what happened - if some exception was triggered etc.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 11:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-startup-problem/m-p/1606818#M22985</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-02-28T11:49:51Z</dc:date>
    </item>
  </channel>
</rss>