<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5644A DSPI CSSCK behaviour</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606110#M22976</link>
    <description>&lt;P&gt;Yes, it is correct behavior, all these times are supposed to be there. The only time disappearing between frames in case continuous transfer, it is tDT.&lt;/P&gt;</description>
    <pubDate>Mon, 27 Feb 2023 13:31:11 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-02-27T13:31:11Z</dc:date>
    <item>
      <title>MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1604589#M22950</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question regarding the DSPI controller in the MPC5644A. I would like to configure a delay between the assertion of the chipselect and the first edge of SCK. When changing CSSCK[0:3] to something &amp;gt;0 I do indeed see a delay between the assertion of PCS and the first edge of SCK. But the same delay is now also present between each 8bit frame! Same goes for ASC[0:3].&lt;/P&gt;&lt;P&gt;Any ideas on what I might be missing? Or is this intended behaviour?&lt;/P&gt;&lt;P&gt;Thanks for your support&lt;/P&gt;</description>
      <pubDate>Thu, 23 Feb 2023 12:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1604589#M22950</guid>
      <dc:creator>kaifalkenberg</dc:creator>
      <dc:date>2023-02-23T12:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1604594#M22951</link>
      <description>&lt;P&gt;  Here are two screenshots illustrating the issue. Between both screenshots only CSSCK has been changed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RigolDS0.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212135iE7667C75E9F1E7C6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RigolDS0.png" alt="RigolDS0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="RigolDS1.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212136i3E5637C0FB80FADF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="RigolDS1.png" alt="RigolDS1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Feb 2023 12:53:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1604594#M22951</guid>
      <dc:creator>kaifalkenberg</dc:creator>
      <dc:date>2023-02-23T12:53:43Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1605986#M22970</link>
      <description>&lt;P&gt;bump&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 09:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1605986#M22970</guid>
      <dc:creator>kaifalkenberg</dc:creator>
      <dc:date>2023-02-27T09:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606110#M22976</link>
      <description>&lt;P&gt;Yes, it is correct behavior, all these times are supposed to be there. The only time disappearing between frames in case continuous transfer, it is tDT.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 13:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606110#M22976</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-27T13:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606195#M22979</link>
      <description>&lt;P&gt;From the RM, chapter 30.9.5.2:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The PCS to SCK delay is the length of time from assertion of the PCS signal to the first SCK edge."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;CS is asserted the entire time..&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 15:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606195#M22979</guid>
      <dc:creator>kaifalkenberg</dc:creator>
      <dc:date>2023-02-27T15:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A DSPI CSSCK behaviour</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606683#M22983</link>
      <description>&lt;P&gt;tCSC will be the always as you can see on the screenshot below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1677572661638.png" style="width: 641px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212610i05B7329651DB948D/image-dimensions/641x691?v=v2" width="641" height="691" role="button" title="davidtosenovjan_0-1677572661638.png" alt="davidtosenovjan_0-1677572661638.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 08:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644A-DSPI-CSSCK-behaviour/m-p/1606683#M22983</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-28T08:24:59Z</dc:date>
    </item>
  </channel>
</rss>