<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5744_Master_Code</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Master-Code/m-p/482320#M2291</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is basically still the same DSPI module as it is used on MPC55xx, MPC56xx and MPC57xx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can offer you simple DSPI example here, chapter 24:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I am attaching example I have written for communication between MPC5676R device (master) and S25FL129P SPI flash memory (slave). Hope it helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Dec 2015 12:59:38 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2015-12-22T12:59:38Z</dc:date>
    <item>
      <title>MPC5744_Master_Code</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Master-Code/m-p/482319#M2290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I am working on MPC5744p EVB. I am trying to&amp;nbsp; implement the SPI Master driver code. Can you please send example(Reference) code for SPI Master.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Dec 2015 11:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-Master-Code/m-p/482319#M2290</guid>
      <dc:creator>swathireddy</dc:creator>
      <dc:date>2015-12-14T11:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744_Master_Code</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744-Master-Code/m-p/482320#M2291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is basically still the same DSPI module as it is used on MPC55xx, MPC56xx and MPC57xx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can offer you simple DSPI example here, chapter 24:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I am attaching example I have written for communication between MPC5676R device (master) and S25FL129P SPI flash memory (slave). Hope it helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 12:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744-Master-Code/m-p/482320#M2291</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2015-12-22T12:59:38Z</dc:date>
    </item>
  </channel>
</rss>