<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: max frequency on MPC5777C</title>
    <link>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1601052#M22892</link>
    <description>&lt;P&gt;OK i try, because i have&amp;nbsp;no other solution to speed up a function&lt;/P&gt;</description>
    <pubDate>Fri, 17 Feb 2023 10:36:56 GMT</pubDate>
    <dc:creator>marcellobellini</dc:creator>
    <dc:date>2023-02-17T10:36:56Z</dc:date>
    <item>
      <title>max frequency on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1597200#M22841</link>
      <description>&lt;P&gt;I would need to increase the frequency of the mpc5777c from 300mhz to 324mhz. My application works in a temperature range of 0-70 degrees.&lt;BR /&gt;it's possible?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 09:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1597200#M22841</guid>
      <dc:creator>marcellobellini</dc:creator>
      <dc:date>2023-02-10T09:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: max frequency on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1598059#M22851</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The max tested and specified frequency for this device is 300MHz. If you run it at higher we will not guarantee its correct operation as specified in datasheet.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 09:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1598059#M22851</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-02-13T09:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: max frequency on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1601052#M22892</link>
      <description>&lt;P&gt;OK i try, because i have&amp;nbsp;no other solution to speed up a function&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 10:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/max-frequency-on-MPC5777C/m-p/1601052#M22892</guid>
      <dc:creator>marcellobellini</dc:creator>
      <dc:date>2023-02-17T10:36:56Z</dc:date>
    </item>
  </channel>
</rss>