<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why is this UID value set to 0 in the example code? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Why-is-this-UID-value-set-to-0-in-the-example-code/m-p/1594424#M22802</link>
    <description>&lt;P&gt;Hi NXP teams&lt;/P&gt;&lt;P&gt;I saw that UID is a unique value for each microcontrollers and it's set on the manufacturing process.&lt;/P&gt;&lt;P&gt;But in the process of the loadkey in the cse example code (cse_keyconfig_mpc5777c), I can see that uid is defined with value 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is this so?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="uid.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209883i260883ADCBF0BDA9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="uid.PNG" alt="uid.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
    <pubDate>Tue, 07 Feb 2023 06:38:23 GMT</pubDate>
    <dc:creator>InhyeokHwang</dc:creator>
    <dc:date>2023-02-07T06:38:23Z</dc:date>
    <item>
      <title>Why is this UID value set to 0 in the example code?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Why-is-this-UID-value-set-to-0-in-the-example-code/m-p/1594424#M22802</link>
      <description>&lt;P&gt;Hi NXP teams&lt;/P&gt;&lt;P&gt;I saw that UID is a unique value for each microcontrollers and it's set on the manufacturing process.&lt;/P&gt;&lt;P&gt;But in the process of the loadkey in the cse example code (cse_keyconfig_mpc5777c), I can see that uid is defined with value 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is this so?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="uid.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209883i260883ADCBF0BDA9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="uid.PNG" alt="uid.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 06:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Why-is-this-UID-value-set-to-0-in-the-example-code/m-p/1594424#M22802</guid>
      <dc:creator>InhyeokHwang</dc:creator>
      <dc:date>2023-02-07T06:38:23Z</dc:date>
    </item>
    <item>
      <title>Re: Why is this UID value set to 0 in the example code?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Why-is-this-UID-value-set-to-0-in-the-example-code/m-p/1594537#M22810</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211495"&gt;@InhyeokHwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is called wildcard UID and it is given by SHE specification.&lt;/P&gt;
&lt;P&gt;All keys can be initially loaded using wildcard UID 0. Each key (except RAM key) have WILDCARD attribute. If you set this bit while loading a key, it's not possible to use wildcard UID anymore for this key. If you keep it '0', wildcard UID can be used also for updates of that key.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 08:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Why-is-this-UID-value-set-to-0-in-the-example-code/m-p/1594537#M22810</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-02-07T08:52:22Z</dc:date>
    </item>
  </channel>
</rss>