<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mpc5777c CSE load key in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593554#M22785</link>
    <description>&lt;P&gt;Hi NXP teams&lt;/P&gt;&lt;P&gt;I'm currently studying on cse_keyconfig_mpc5777c example code from s32 ds pa 2.1 and I found something strange in the code which I don't get it.&lt;/P&gt;&lt;P&gt;According to the reference manual, all M1, M2, M3, M4, M5 should be computed and used for the load key command.&lt;/P&gt;&lt;P&gt;But in the example code, I only can see computeM1M2M3 function inside load key command and have no idea why computeM4M5 is not being used.&lt;/P&gt;&lt;P&gt;When I try to find the usage of computeM4M5 in the project using ctrl+h, this function is used nowhere.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Mon, 06 Feb 2023 02:30:11 GMT</pubDate>
    <dc:creator>InhyeokHwang</dc:creator>
    <dc:date>2023-02-06T02:30:11Z</dc:date>
    <item>
      <title>mpc5777c CSE load key</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593554#M22785</link>
      <description>&lt;P&gt;Hi NXP teams&lt;/P&gt;&lt;P&gt;I'm currently studying on cse_keyconfig_mpc5777c example code from s32 ds pa 2.1 and I found something strange in the code which I don't get it.&lt;/P&gt;&lt;P&gt;According to the reference manual, all M1, M2, M3, M4, M5 should be computed and used for the load key command.&lt;/P&gt;&lt;P&gt;But in the example code, I only can see computeM1M2M3 function inside load key command and have no idea why computeM4M5 is not being used.&lt;/P&gt;&lt;P&gt;When I try to find the usage of computeM4M5 in the project using ctrl+h, this function is used nowhere.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 02:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593554#M22785</guid>
      <dc:creator>InhyeokHwang</dc:creator>
      <dc:date>2023-02-06T02:30:11Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5777c CSE load key</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593694#M22788</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211495"&gt;@InhyeokHwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the thing is that M1-M3 are input parameters needed to load a key, M4-M5 values are output values.&lt;/P&gt;
&lt;P&gt;M4-M5 values should be used to verify if a key was loaded correctly. If returned M4-M5 values match with M4-M5 values calculated offline, it's a proof that the key was loaded correctly. In the real application, it's highly recommended to do this checking, of course. Project cse_keyconfig_mpc5777c is example only, it's not implemented for some reasons.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 07:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593694#M22788</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-02-06T07:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5777c CSE load key</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593721#M22789</link>
      <description>&lt;P&gt;thanks for the reply. I appreciate it&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 07:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-CSE-load-key/m-p/1593721#M22789</guid>
      <dc:creator>InhyeokHwang</dc:creator>
      <dc:date>2023-02-06T07:34:18Z</dc:date>
    </item>
  </channel>
</rss>