<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570583#M22508</link>
    <description>&lt;P&gt;Thanks for explaining. Which document is Your screenshot taken from, please? Because I need to identify all eMIOS channels with this feature ...&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 16:40:26 GMT</pubDate>
    <dc:creator>martinklonfar</dc:creator>
    <dc:date>2022-12-15T16:40:26Z</dc:date>
    <item>
      <title>Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1569739#M22503</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;On MPC5777C, I need to use eMIOS5 in SAIC mode. However, when I assign the eMIOS-function to the pin (SIU_PCR184 = 0x0503), the input signal almost disappears and eMIOS5 never detects any edge. Checking the pin with multimeter I found out that its resistance against GND drops to some 14-15 Ohm after assigning the eMIOS-function - hence the "disappearance" of the input signal.&lt;/P&gt;&lt;P&gt;Temporary re-wiring to eMIOS23 solved the issue, but that's not a long-term option.&lt;/P&gt;&lt;P&gt;Is it possible to use the eMIOS-input function on this pin?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 13:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1569739#M22503</guid>
      <dc:creator>martinklonfar</dc:creator>
      <dc:date>2022-12-14T13:19:23Z</dc:date>
    </item>
    <item>
      <title>Re: Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570243#M22506</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;no, it is not possible to use pin for eMIOS input, it is output only pin&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1671090719449.png" style="width: 576px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204550i605C77E3B9D1DFCC/image-dimensions/576x52?v=v2" width="576" height="52" role="button" title="PetrS_0-1671090719449.png" alt="PetrS_0-1671090719449.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 07:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570243#M22506</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-12-15T07:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570583#M22508</link>
      <description>&lt;P&gt;Thanks for explaining. Which document is Your screenshot taken from, please? Because I need to identify all eMIOS channels with this feature ...&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 16:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570583#M22508</guid>
      <dc:creator>martinklonfar</dc:creator>
      <dc:date>2022-12-15T16:40:26Z</dc:date>
    </item>
    <item>
      <title>Re: Pin eMIOS5/eTPUA5/GPIO184 can't be used as eMIOS-input?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570686#M22509</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;words from RM's chapter 3.5&amp;nbsp;External signal descriptions, multiplexing, and attributes...&lt;BR /&gt;Details about external signal functions, their static electrical characteristics, and pad configuration settings for this chip appear in the spreadsheet that is embedded within this document:&lt;BR /&gt;MPC5777C_System_IO_Definition.xlsx&lt;BR /&gt;To access this spreadsheet, view the document's list of attachments.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1671133491226.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204640iC143D15CBA97CF88/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1671133491226.png" alt="PetrS_0-1671133491226.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 19:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Pin-eMIOS5-eTPUA5-GPIO184-can-t-be-used-as-eMIOS-input/m-p/1570686#M22509</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-12-15T19:45:56Z</dc:date>
    </item>
  </channel>
</rss>