<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Check for errors on ethernet driver in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Check-for-errors-on-ethernet-driver/m-p/1548807#M22293</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can enable error interrupt in the enet component. Then when error is detected a configured callback is called with&amp;nbsp;ENET_ERR_EVENT event. You can read interrupt flags using&amp;nbsp;ENET_DRV_GetInterruptFlags to see what kind of errors was detected.&amp;nbsp;&lt;BR /&gt;Also Enet module includes statistic and error counters so it can be used to monitor&amp;nbsp;&lt;SPAN&gt;for frame traffic and errors. Counters are enabled by&amp;nbsp;ENET_DRV_ConfigCounters and individual counters can be read using&amp;nbsp;ENET_DRV_GetCounter. Or you can check those counters in debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Nov 2022 09:27:03 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-11-04T09:27:03Z</dc:date>
    <item>
      <title>Check for errors on ethernet driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Check-for-errors-on-ethernet-driver/m-p/1545717#M22255</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to check if there are any errors on the ethernet interface?&lt;/P&gt;&lt;P&gt;SDK S32_SDK_S32PA_RTM_3.0.3&lt;/P&gt;</description>
      <pubDate>Fri, 28 Oct 2022 14:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Check-for-errors-on-ethernet-driver/m-p/1545717#M22255</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2022-10-28T14:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: Check for errors on ethernet driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Check-for-errors-on-ethernet-driver/m-p/1548807#M22293</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can enable error interrupt in the enet component. Then when error is detected a configured callback is called with&amp;nbsp;ENET_ERR_EVENT event. You can read interrupt flags using&amp;nbsp;ENET_DRV_GetInterruptFlags to see what kind of errors was detected.&amp;nbsp;&lt;BR /&gt;Also Enet module includes statistic and error counters so it can be used to monitor&amp;nbsp;&lt;SPAN&gt;for frame traffic and errors. Counters are enabled by&amp;nbsp;ENET_DRV_ConfigCounters and individual counters can be read using&amp;nbsp;ENET_DRV_GetCounter. Or you can check those counters in debugger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 09:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Check-for-errors-on-ethernet-driver/m-p/1548807#M22293</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-11-04T09:27:03Z</dc:date>
    </item>
  </channel>
</rss>