<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CRC32 array calculation in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CRC32-array-calculation/m-p/1547791#M22283</link>
    <description>&lt;P&gt;Hello, I want to learn how an array calculates crc. For example, the CRC32 result of { 0x94 0x90 } array is 0xA4FBCEA5 in my code. Also, the CRC32 result of { 0x90 0x94 } array is 0xC7FACFB8 in my code.&lt;/P&gt;&lt;P&gt;How to calculate CRC. Does it calculate the crc of each value one by one and then performs a transaction between all of them?&lt;BR /&gt;What are the processes that take place in the background in crc calculation, can you explain the stages?&lt;/P&gt;&lt;P&gt;For example, it gives a single crc value whether the number of data is 2 or 100.&lt;/P&gt;&lt;P&gt;0x7C, 0x00, 0x01, 0x46, 0x70, 0x60, 0x00, 0x00, 0x7C, 0x74, 0x53, 0xA6, 0x70, 0x60, 0x02, 0x01 = 0x907ACA68&lt;/P&gt;&lt;P&gt;0x7C, 0x00 = 0xC2532405&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(My board MPC5777C-516)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all answers &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Nov 2022 14:30:59 GMT</pubDate>
    <dc:creator>safa1999</dc:creator>
    <dc:date>2022-11-02T14:30:59Z</dc:date>
    <item>
      <title>CRC32 array calculation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CRC32-array-calculation/m-p/1547791#M22283</link>
      <description>&lt;P&gt;Hello, I want to learn how an array calculates crc. For example, the CRC32 result of { 0x94 0x90 } array is 0xA4FBCEA5 in my code. Also, the CRC32 result of { 0x90 0x94 } array is 0xC7FACFB8 in my code.&lt;/P&gt;&lt;P&gt;How to calculate CRC. Does it calculate the crc of each value one by one and then performs a transaction between all of them?&lt;BR /&gt;What are the processes that take place in the background in crc calculation, can you explain the stages?&lt;/P&gt;&lt;P&gt;For example, it gives a single crc value whether the number of data is 2 or 100.&lt;/P&gt;&lt;P&gt;0x7C, 0x00, 0x01, 0x46, 0x70, 0x60, 0x00, 0x00, 0x7C, 0x74, 0x53, 0xA6, 0x70, 0x60, 0x02, 0x01 = 0x907ACA68&lt;/P&gt;&lt;P&gt;0x7C, 0x00 = 0xC2532405&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(My board MPC5777C-516)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all answers &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 14:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CRC32-array-calculation/m-p/1547791#M22283</guid>
      <dc:creator>safa1999</dc:creator>
      <dc:date>2022-11-02T14:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: CRC32 array calculation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CRC32-array-calculation/m-p/1551824#M22325</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;you can take a look at this example:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-CRC32-GHS614/ta-p/1119736" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-CRC32-GHS614/ta-p/1119736&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It's written for MPC5748G but there's the same CRC module on MPC5777C.&lt;/P&gt;
&lt;P&gt;Anytime you write input register, output register is updated and contains CRC of data stream you already wrote there.&lt;/P&gt;
&lt;P&gt;I believe the example will help to understand how it works.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 08:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CRC32-array-calculation/m-p/1551824#M22325</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-11-10T08:53:37Z</dc:date>
    </item>
  </channel>
</rss>