<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1525761#M22019</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;If you don't want to use RTOS, then Bare-metal embedded system approach is a choice.&lt;BR /&gt;Setup your Stack inside a task within a super loop :&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 21 Sep 2022 09:51:19 GMT</pubDate>
    <dc:creator>cuongnguyenphu</dc:creator>
    <dc:date>2022-09-21T09:51:19Z</dc:date>
    <item>
      <title>Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1524239#M22002</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I am working on MPC5777C microcontroller. We have used EB Tresos tool to configure the ethernet driver.&lt;/P&gt;&lt;P&gt;We are looking for Classic AUTOSAR compliant TCP/IP stack without FreeRTOS for implementing the bootloader that uses the Ethernet interface.&lt;/P&gt;&lt;P&gt;Please suggest the best way without RTOS.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ajmeri Jaimin&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 10:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1524239#M22002</guid>
      <dc:creator>ajmerijaimin</dc:creator>
      <dc:date>2022-09-19T10:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1525761#M22019</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;If you don't want to use RTOS, then Bare-metal embedded system approach is a choice.&lt;BR /&gt;Setup your Stack inside a task within a super loop :&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 09:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1525761#M22019</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2022-09-21T09:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1525780#M22022</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195919"&gt;@cuongnguyenphu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I now have this perception of the super loop. I will check further to understand how to compile it. I have a question. Is the stack AUTOSAR compliant? can you please confirm?&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 10:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1525780#M22022</guid>
      <dc:creator>ajmerijaimin</dc:creator>
      <dc:date>2022-09-21T10:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1527951#M22059</link>
      <description>&lt;P&gt;It depends on how you implemented in that super loop. NXP package for MPC only focus on Autosar MCAL layer, while TCP/IP stack is placed between Socket Adaptor and EthIf layer.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cuongnguyenphu_0-1664179173851.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194882iA5D6A307E19ABE82/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cuongnguyenphu_0-1664179173851.png" alt="cuongnguyenphu_0-1664179173851.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;cuongnguyenphu_0-1664179173851.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Can you refer these topics below for some solution of FNET and LwIP to use TCP/IP stack. But I'm not sure about the Autosar compliant of these solutions:|&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/does-anybody-have-a-TCPIP-library-compiled-for-MPC5775k-or/m-p/636997" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/does-anybody-have-a-TCPIP-library-compiled-for-MPC5775k-or/m-p/636997&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/AUTOSAR-TCP-IP-stack/m-p/925261" target="_blank"&gt;https://community.nxp.com/t5/S32K/AUTOSAR-TCP-IP-stack/m-p/925261&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 07:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1527951#M22059</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2022-09-26T07:59:46Z</dc:date>
    </item>
    <item>
      <title>Re: Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1539372#M22177</link>
      <description>&lt;P&gt;Just an update.&lt;/P&gt;&lt;P&gt;I've ported LWIP for our project and I've used it NO_SYS for bare-metal. It's working fine with MCAL drivers.&lt;/P&gt;&lt;P&gt;We are aware that LWIP is not AUTOSAR compliant. I think it's best to keep AUTOSAR compliant aside and continue to work on the remaining stuff. Because I belive the stack can be swapped later.&lt;/P&gt;&lt;P&gt;Thanks for the support.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 13:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-AUTOSAR-TCP-IP-stack-without-FreeRTOS-on-MPC5777C/m-p/1539372#M22177</guid>
      <dc:creator>ajmerijaimin</dc:creator>
      <dc:date>2022-10-18T13:56:10Z</dc:date>
    </item>
  </channel>
</rss>