<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing mode changing in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493251#M21602</link>
    <description>&lt;P&gt;Yes, that's correct. It just does not support elf files but rather s-record files or hex files. Here you can find how to generate such file in S32 Design Studio:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Generate-S-Record-Intel-HEX-Binary-file/ta-p/1105838" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Generate-S-Record-Intel-HEX-Binary-file/ta-p/1105838&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Thu, 21 Jul 2022 09:57:33 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2022-07-21T09:57:33Z</dc:date>
    <item>
      <title>Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1490764#M21541</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can we change flashing mode of MPC5775B board with CAN medium. If yes, then what are the requirements for that.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 05:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1490764#M21541</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-07-18T05:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1491820#M21568</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I just answered similar question from your company via ticket. Let me copy the answer here:&lt;/P&gt;
&lt;P&gt;***&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There are more options how to implement a bootloader on this device. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you want to use serial boot mode (using BAM module), there are two ways how to switch to serial boot mode:&lt;/SPAN&gt;&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;&lt;SPAN&gt; Change BOOTCFG pins as needed. The pins are latched during reset. So, you need to have an option to change this state by hardware (jumpers, pushbutton or whatever). &lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt; Second option is to change the mode by DCF record. See “&lt;/SPAN&gt;5.7.1 UTEST Miscellaneous DCF client” in the reference manual for more details.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;However, it’s not very common solution to use this serial boot mode. Absolute majority of our customers use rather flash resident bootloader.&lt;/P&gt;
&lt;P&gt;We provide Rappid bootloader which can use either UART or CAN. At the beginning, it’s necessary to load RBF file to flash via JTAG. Notice that we do not provide source codes, it cannot be modified:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Some custom RBF files can be downloaded here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/RAppID-Bootloader-custom-rbf-files/ta-p/1115140" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/RAppID-Bootloader-custom-rbf-files/ta-p/1115140&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Then we provide application note AN5319 which describes how to develop simple serial bootloader. SW example is included. It’s written for MPC5748G but it’s supposed to be starting point for all MPC57xx devices:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5319.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5319.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are looking for out of box solution, you can ask Vector (or other SW vendors) for help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.vector.com/int/en/products/products-a-z/embedded-components/flash-bootloader" target="_blank"&gt;https://www.vector.com/int/en/products/products-a-z/embedded-components/flash-bootloader#&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 13:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1491820#M21568</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-07-19T13:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493026#M21586</link>
      <description>&lt;P&gt;Can i use RBF file of MPC5777C&amp;nbsp; for MPC5775B board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 05:40:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493026#M21586</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-07-21T05:40:06Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493031#M21587</link>
      <description>&lt;P&gt;Yes, the devices are compatible.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 06:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493031#M21587</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-07-21T06:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493045#M21588</link>
      <description>&lt;P&gt;ok, correct me if i'm wrong. 1) I have to load RBF file to MPC5775B board via JTAG . 2) after loading RBF then I use CAN communication for flashing .elf file via RAppid bootloader.&lt;/P&gt;&lt;P&gt;is it correct way?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 06:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493045#M21588</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-07-21T06:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493251#M21602</link>
      <description>&lt;P&gt;Yes, that's correct. It just does not support elf files but rather s-record files or hex files. Here you can find how to generate such file in S32 Design Studio:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Generate-S-Record-Intel-HEX-Binary-file/ta-p/1105838" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Generate-S-Record-Intel-HEX-Binary-file/ta-p/1105838&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 09:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493251#M21602</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-07-21T09:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493281#M21607</link>
      <description>&lt;P&gt;ok but i'm using matlab&amp;nbsp; and i want to run application using matlab(MBD). so how can i generate hex file in matlab&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 10:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493281#M21607</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-07-21T10:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493394#M21610</link>
      <description>&lt;P&gt;It was already discussed here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-create-bin-hex-s19-file-using-the-MBD-tool-for-S32/m-p/673008/highlight/true" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-create-bin-hex-s19-file-using-the-MBD-tool-for-S32/m-p/673008/highlight/true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If it does not answer your questions, please use this community space:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 14:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1493394#M21610</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-07-21T14:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1494478#M21626</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;I'm trying to build MPC5777C RBF file into MPC5775B through s32ide but I'm getting flashing error like "Error during flash programming terminating debug session".&amp;nbsp; I'm using JTAG here for flashing.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 05:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1494478#M21626</guid>
      <dc:creator>saurabhkulkarni123</dc:creator>
      <dc:date>2022-07-25T05:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing mode changing</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1498536#M21703</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;did you do that using these steps?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 06:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flashing-mode-changing/m-p/1498536#M21703</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-08-01T06:02:51Z</dc:date>
    </item>
  </channel>
</rss>