<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: CAN_RX pin state</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476066#M2116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for replying.&lt;/P&gt;&lt;P&gt;However what we have observed is that the bus-off does not happen always. It happens only sometimes although we transmit always. So, what we observe is that the bus-off behaviour occurs sometimes.&lt;/P&gt;&lt;P&gt;One thing what we plan to do is to enable the weak pull-down available in the MPC5646C microcontroller for CAN_RX. Atleast with this we do not see bus-off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jagadish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Mar 2016 10:06:49 GMT</pubDate>
    <dc:creator>Jagadish</dc:creator>
    <dc:date>2016-03-12T10:06:49Z</dc:date>
    <item>
      <title>CAN_RX pin state</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476064#M2114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question related to CAN hardware in microcontroller MPC5646C.&lt;/P&gt;&lt;P&gt;For some specific reasons we have in our hardware a CAN controller which is started and CAN messages being transmitted. The CAN_TX and CAN_RX lines are not connected to any transceiver and are left open. In this situation, when we transmit we see that there is a bus-off occurring although we have configured CAN_RX pin as CAN specific receive functional pin.&lt;/P&gt;&lt;P&gt;Is this bus-off expected if the CAN lines are left open but correctly configured in software?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jagadish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Feb 2016 07:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476064#M2114</guid>
      <dc:creator>Jagadish</dc:creator>
      <dc:date>2016-02-20T07:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_RX pin state</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476065#M2115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, this is expected behavior. If the FlexCAN sees the RX pin high, it can synchronizes to the bus , thus it is able to transmit a message. However, because of unconnected TX/RX pins, the FlexCAN does not receive what it is transmitted and so a bit error occurs. An error frame is transmitted, again with a bit error. This is repeated until bus error happen.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 07:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476065#M2115</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-02-22T07:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_RX pin state</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476066#M2116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for replying.&lt;/P&gt;&lt;P&gt;However what we have observed is that the bus-off does not happen always. It happens only sometimes although we transmit always. So, what we observe is that the bus-off behaviour occurs sometimes.&lt;/P&gt;&lt;P&gt;One thing what we plan to do is to enable the weak pull-down available in the MPC5646C microcontroller for CAN_RX. Atleast with this we do not see bus-off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jagadish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Mar 2016 10:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-RX-pin-state/m-p/476066#M2116</guid>
      <dc:creator>Jagadish</dc:creator>
      <dc:date>2016-03-12T10:06:49Z</dc:date>
    </item>
  </channel>
</rss>