<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Send 32-bit SPI</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452709#M21112</link>
    <description>&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
    <pubDate>Wed, 04 May 2022 12:24:11 GMT</pubDate>
    <dc:creator>CHAOWeiXu</dc:creator>
    <dc:date>2022-05-04T12:24:11Z</dc:date>
    <item>
      <title>Send 32-bit SPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1451302#M21085</link>
      <description>&lt;P&gt;hi，&lt;/P&gt;&lt;P class="lia-align-left"&gt;I use the MPC5744P SPI module.It uses 16 bit SPI to send, but I want it to send 32 bits.I try to manually control the CS to send 32 bits.But the SCK signal will be delayed when it is sent. I want to send two 16 bits in a row.&lt;/P&gt;&lt;P class="lia-align-left"&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 11:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1451302#M21085</guid>
      <dc:creator>CHAOWeiXu</dc:creator>
      <dc:date>2022-04-29T11:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: Send 32-bit SPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452161#M21104</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;what code do you use for this? Some delay can be caused by SW delay, also by HW (see CTAR setting).&lt;BR /&gt;Manual control of CS is not needed, module is able to do that, if need CS low between words use continuous selection format, check chapter&amp;nbsp;49.4.4.5 Continuous Selection Format of the RM.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 May 2022 08:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452161#M21104</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-05-03T08:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: Send 32-bit SPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452300#M21109</link>
      <description>&lt;P&gt;hi,Mr,Petr&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I use Simulink to build the model. Its name is NXP_ MBDToolbox_ MPC57xx.&lt;/P&gt;&lt;P&gt;I want the master to send 32-bit data to the slave, but it only supports sending 16-bit data.&lt;/P&gt;&lt;P&gt;When I adjust the transfer size to 32, the oscilloscope displays abnormal.When I adjust the transfer size to 16, if I send 16 bits twice in a row, there will be a delay between SCKs.In the attachment are my model and the oscilloscope image when it is sent twice in a row.&lt;/P&gt;&lt;P&gt;Thanks，&lt;/P&gt;</description>
      <pubDate>Tue, 03 May 2022 15:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452300#M21109</guid>
      <dc:creator>CHAOWeiXu</dc:creator>
      <dc:date>2022-05-03T15:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: Send 32-bit SPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452659#M21111</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if using MATLAB/Simulink with toolbox please ask question directly on its Community space;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 10:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452659#M21111</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-05-04T10:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: Send 32-bit SPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452709#M21112</link>
      <description>&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 12:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Send-32-bit-SPI/m-p/1452709#M21112</guid>
      <dc:creator>CHAOWeiXu</dc:creator>
      <dc:date>2022-05-04T12:24:11Z</dc:date>
    </item>
  </channel>
</rss>