<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The address for flexray modle on MPC 5744P in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1450461#M21056</link>
    <description>&lt;P&gt;Hi could you share your flexray drivers with me, thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Apr 2022 06:40:37 GMT</pubDate>
    <dc:creator>Wangerxi</dc:creator>
    <dc:date>2022-04-28T06:40:37Z</dc:date>
    <item>
      <title>The address for flexray modle on MPC 5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1057536#M15870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am tring to develop the flexray model on MPC 5744P,and I take the driveer code for MPC 5604P as a reference . There are two nodes in the communication net ，the two nodes can establish a communication loop，the waveform can be seen in the oscilloscope，but I can't transmit or receive any messages.I hope some can help me .&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;two question : First, I detect the CHI Error Flag Register（FR_CHIERFR）and find that the bit ILSA_EF is 1.I found the reason as show in the picture below， but I don’t know how to correct it，I set 0x40004000 asthe flexray memory address ，but I don't know it is right or not. Second there is no &lt;SPAN class=""&gt;Message Buffer Data Field Offset Register (FR_MBDOR&lt;/SPAN&gt;&lt;SPAN class=""&gt;n&lt;/SPAN&gt;&lt;SPAN class=""&gt;)&amp;nbsp;&lt;/SPAN&gt;in MPC 5604 for data field offset ,so I don't know how to&amp;nbsp;Calculation the data field offset.&lt;span class="lia-inline-image-display-wrapper" image-alt="3d5baab14726dd71c21660263def313.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109227iC3A896A0D1978AC4/image-size/large?v=v2&amp;amp;px=999" role="button" title="3d5baab14726dd71c21660263def313.png" alt="3d5baab14726dd71c21660263def313.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Aug 2020 01:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1057536#M15870</guid>
      <dc:creator>957263248</dc:creator>
      <dc:date>2020-08-23T01:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: The address for flexray modle on MPC 5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1133048#M16518</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is a response I got from Apps team...&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"The address should be configured correctly – it is in system memory RAM range. Do you have initialized the system RAM memory in startup?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Mainly the issue will be that you don’t have configured the MBDORn Data Field offsets registers (“ILSA_EF: The CC detects the usage of an data field offset with value of 0“, see also chapter 50.8.1.2 Configure Data Field Offsets where is mentioned that the ILSA_EF is generated when the registers are not configured).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The data field offset is calculate as below on MPC5744P&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How to get the address of the MB Header:&lt;/P&gt;
&lt;P&gt;SADR_MBHF[n] = SMBA + MBIDXR(n)[MBIDX]*8&lt;/P&gt;
&lt;P&gt;How to get the address of the MB data:&lt;/P&gt;
&lt;P&gt;SADR_MBDF[n] = SMBA + MBDOR(i) = SMBA + MBDOR(MBIDXR(n)[MBIDX])"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 10:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1133048#M16518</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-01T10:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: The address for flexray modle on MPC 5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1450461#M21056</link>
      <description>&lt;P&gt;Hi could you share your flexray drivers with me, thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Apr 2022 06:40:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/The-address-for-flexray-modle-on-MPC-5744P/m-p/1450461#M21056</guid>
      <dc:creator>Wangerxi</dc:creator>
      <dc:date>2022-04-28T06:40:37Z</dc:date>
    </item>
  </channel>
</rss>