<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN/FlexCAN Loopback test in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CAN-FlexCAN-Loopback-test/m-p/1432900#M20752</link>
    <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;I am modify examples both in "can_pal_mpc5748G" and "flexcan_mpc5748G" from SDA_PA_RTM_V3.0.3 to perform loopback test.&amp;nbsp; However, it does not seem to work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For loopback mode, I changed the operation mode to "Loop Back" in CAN/FLEXCAN component.&amp;nbsp; Also, I created a timer interrupt to send out the CAN message every 2 seconds.&amp;nbsp; But, there is no message being loop back from Rx end.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did do something wrong????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;James&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 20:26:30 GMT</pubDate>
    <dc:creator>karma_JC</dc:creator>
    <dc:date>2022-03-23T20:26:30Z</dc:date>
    <item>
      <title>CAN/FlexCAN Loopback test</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-FlexCAN-Loopback-test/m-p/1432900#M20752</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;I am modify examples both in "can_pal_mpc5748G" and "flexcan_mpc5748G" from SDA_PA_RTM_V3.0.3 to perform loopback test.&amp;nbsp; However, it does not seem to work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For loopback mode, I changed the operation mode to "Loop Back" in CAN/FLEXCAN component.&amp;nbsp; Also, I created a timer interrupt to send out the CAN message every 2 seconds.&amp;nbsp; But, there is no message being loop back from Rx end.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did do something wrong????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;James&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 20:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-FlexCAN-Loopback-test/m-p/1432900#M20752</guid>
      <dc:creator>karma_JC</dc:creator>
      <dc:date>2022-03-23T20:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/FlexCAN Loopback test</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-FlexCAN-Loopback-test/m-p/1433304#M20762</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;loopback mode is normally functional. Do you have set a receive message buffer to receive transmitted ID? In example easily have same value for both&amp;nbsp;TX_MSG_ID and RX_MSG_ID.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 08:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-FlexCAN-Loopback-test/m-p/1433304#M20762</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-03-24T08:35:16Z</dc:date>
    </item>
  </channel>
</rss>