<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EQADC output in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1430590#M20702</link>
    <description>&lt;P&gt;What is the voltage you are converting? Is it is stabilized output of laboratory power supply?&lt;/P&gt;
&lt;P&gt;Also you are converting without calibration, convert WITH calibration.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Mar 2022 08:45:27 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2022-03-18T08:45:27Z</dc:date>
    <item>
      <title>EQADC output</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1429255#M20682</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm currently working on MPC5777C, In this I'm using EQADC to read voltage.&lt;/P&gt;&lt;P&gt;As per the spec and some reference program from the forum made a program.&lt;/P&gt;&lt;P&gt;I'm also getting the output, however the issue is there is a huge variations in the output .&lt;/P&gt;&lt;P&gt;Attached the output image of EQADC_A.&lt;/P&gt;&lt;P&gt;and also attached the program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;/*
 * main implementation: use this 'C' sample to create your own application
 *
 */

#include "derivative.h" /* include peripheral declarations */

#include &amp;lt;string.h&amp;gt;
#include &amp;lt;stdio.h&amp;gt;

#include "eQADC_macros_MAMBA.h"
#include "D_UART.h"


#define IDEAL_RES75 0x3000	// Ideal value of 75%(VDH-VDL)
#define IDEAL_RES25 0x1000	// Ideal value of 25%(VDH-VDL)


#define APC 0x2000
#define OBE 0x0200
#define IBE 0x0100
#define ODE 0x0020
#define SRC 0x0004
#define WPE 0x0002
#define WPS 0x0001
#define ALT0 0x0000
#define ALT1 0x0400
#define ALT2 0x0800
#define ALT3 0x0C00


#define ANB16_pin 484 // PCR number
#define ANB17_pin 485
#define ANB18_pin 486
#define ANB19_pin 487

#define ANA29_chnl 29 // channel number
#define ANA18_chnl 18
#define ANA19_chnl 19
#define ANA20_chnl 20

//   Conversion Command Format for the Standard Configuration
#define ANA29_command \
( EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA29_chnl) )
#define ANA18_command \
( EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA18_chnl) )
#define ANA19_command \
( EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA19_chnl) )
#define ANA20_command \
( EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA20_chnl) )


#define ANA17_command_cal \
( CAL | EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA17_chnl) )
#define ANA18_command_cal \
( CAL | EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA18_chnl) )
#define ANA19_command_cal \
( CAL | EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA19_chnl) )
#define ANA20_command_cal \
( CAL | EOQ | MESSAGE_TAG(RFIFO0) | CHANNEL(ANA20_chnl) )





extern void xcptn_xmpl(void);

static void HW_init(void);

static uint32_t Result = 0;

char str[10u] = "receive\n";

static void HW_init(void)
{
    /* set round robin for all slaves */
    XBAR.PORT[0].CRS.B.ARB = 1;
    XBAR.PORT[1].CRS.B.ARB = 1;
    XBAR.PORT[2].CRS.B.ARB = 1;
    XBAR.PORT[3].CRS.B.ARB = 1;
    XBAR.PORT[4].CRS.B.ARB = 1;
    XBAR.PORT[6].CRS.B.ARB = 1;
    XBAR.PORT[7].CRS.B.ARB = 1;

}


void D_PLL_Init()
{
// Disable PLL0
  PLLDIG.PLL0CR.R = 0;
// Disable PLL1
  PLLDIG.PLL1CR.R = 0;

// Select XOSC as PLL0 source
// Select PHI1 output of PLL0 as PLL1 source
  SIU.SYSDIV.R = 0x04000010;

 /* Program PLL0
 RFDPHI1 = 0x0C
 RFDPHI = 0x03
 PREDIV = 0x5
 MFD = 0x48
*/
  PLLDIG.PLL0DV.R = 0x60035048;

  //PLLDIG.PLL0DV.R = 0x40025060; //20 MHz crystal

// Wait for stable XOSC
   while (!SIU.RSR.B.XOSC);
 // Turn on PLL0 and wait for lock
   PLLDIG.PLL0CR.R = 0x0300;
   while (!PLLDIG.PLL0SR.B.LOCK);

/* Program PLL1
  RFDPHI = 0x02
  MFD = 0x16
*/
   PLLDIG.PLL1DV.R=0x00020016;
// Turn on PLL1 and wait for lock
   PLLDIG.PLL1CR.R = 0x0300;
   while (!PLLDIG.PLL1SR.B.LOCK);

/*
#******************************
# Select clock dividers and sources
#   PLL0 ref = XOSX
#   PLL1 ref = PLL0 PHI1
#   PERCLKSEL = PLL1
#   PERDIV = Divide-by-2
#   MCANSEL = XOSC
#   SYSCLKSEL = PLL1
#   ETPUDIV = Divide-by-1
#   SYSCLKDIV = Divide-by-1
#   PCS = Disabled
#******************************
*/
 SIU.SYSDIV.R = 0x05002110;
 SIU.ECCR.B.ECCS  = 0;
 SIU.ECCR.B.ENGDIV = 64;

}


static uint32_t ConvertChannel(int32_t channel, int32_t bCal)
{
    uint32_t ret = 0;

    /* Conversion command: convert "channel" */
    /* with ADC0, set EOQ, and send result to RFIFO 0 */
    /* 128 adc clocks sampling */
    EQADC_A.CFPR[0].R = 0x800C0000 | (channel&amp;lt;&amp;lt;8) | (bCal&amp;lt;&amp;lt;24);
    EQADC_A.CFCR0.R = 0x04100000;   /* Trigger CFIFO 0 using Single Scan SW mode */
    /* Wait for RFIFO 0's Drain Flag to set */
    while (EQADC_A.FISR[0].B.RFDFX != 1){}

    ret = EQADC_A.RFPR[0].R;

    /* Clear RFIFO 0's Drain Flag */
    /* Clear CFIFO's End of Queue flag */
    /* RFDF + EOQF */
    EQADC_A.FISR[0].R = 0x10020000;

    return ret;
}

int Compare (const void * p0, const void * p1)
{
    uint32_t a0 = (uint32_t) *(uint32_t*)p0;
    uint32_t a1 = (uint32_t) *(uint32_t*)p1;

    if(a0==a1) return 0;
    if(a0&amp;lt;a1) return -1;
    else return 1;
}

static uint32_t ConvertChannel_Median(int32_t channel, int32_t bCal)
{
    uint32_t results[21];

    int32_t i = 0;
    for(i=0;i&amp;lt;sizeof(results)/sizeof(results[0]);i++)
    {
        results[i] = ConvertChannel(channel, bCal);
    }

    /* sort results */
    qsort((void*)results,21,sizeof(results[i]),Compare);

    return results[10]; /* median */
}





static int32_t EQADC_PowerUpCalibration(void)
{
    unsigned long raw_res75, raw_res25;
    unsigned long cal_res75, cal_res25;

    float gccf, occf;

    unsigned short gain;
    short offset;

    /* Convert channel 43 (75%VRH)with CAL=0 */
    raw_res75 = ConvertChannel_Median(43,0);
    /* Convert channel 44 (25%VRH)with CAL=0, 64 sample time (errata) */
    raw_res25 = ConvertChannel_Median(44,0);

    /* Compute Gain and Offset */
    gccf = (float)(8192.0)/(raw_res75 - raw_res25);
    gain = gccf * 16384;
    occf = (float)(IDEAL_RES75 - (gccf * raw_res75) - 2.0);
    offset = occf;

    /* now store Gain in ADCn_GCCR */
    EQADC_A.CFPR[0].R = (gain&amp;lt;&amp;lt;8) | 0x00000004;
    /* now store offset in ADCn_OCCR */
    EQADC_A.CFPR[0].R = ((unsigned short)offset &amp;lt;&amp;lt;  | 0x00000005;

    /* now store Gain in ADCn_AGR */
    EQADC_A.CFPR[0].R = (gain&amp;lt;&amp;lt;8) | 0x00000031;
    /* now store offset in ADCn_ACR */
    EQADC_A.CFPR[0].R = ((unsigned short)offset &amp;lt;&amp;lt;  | 0x00000032 | 0x80000000;

    EQADC_A.CFCR0.R = 0x04100000;    /* Trigger CFIFO 0 using Single Scan SW mode */
    while (EQADC_A.FISR[0].B.EOQFX !=1) {} /* Wait for End Of Queue flag */
    EQADC_A.FISR[0].R = 0x10000000;

    cal_res75 = ConvertChannel(43,1);
    cal_res25 = ConvertChannel(44,1);

    // Check the results
    if ((abs(cal_res75 - IDEAL_RES75) &amp;gt; 0xF) || (abs(cal_res25 - IDEAL_RES25) &amp;gt; 0xF))
    {
	    /* error */
	    return 1;
    }

    return 0; /* no error */
}



static void eQADCA_init(void)
{

    #define SINGLE_SCAN_TRIGGER_Q0 EQADC_A.CFCR0.R=0x04100000
    #define SINGLE_SCAN_TRIGGER_Q1 EQADC_A.CFCR0.R=0x00000410

    #define EQADC_A_IDCR_PIE_MASK      0x2000
    #define EQADC_A_IDCR_EOQIE_MASK    0x1000
    #define EQADC_A_IDCR_CFFE_MASK     0x0200
    #define EQADC_A_IDCR_CFFS_MASK     0x0100
    #define EQADC_A_IDCR_RFDE_MASK     0x0002
    #define EQADC_A_IDCR_RFDS_MASK     0x0001

    #define FISR_EOQ_MASK 0x10000000

    int32_t i = 0;
    uint32_t res = 0;
    vint32_t counter = 0;

    // expecting per_clk = 96 MHz (PLL0/2 = 192/2)
    // fADC &amp;lt; 16.5MHz =&amp;gt; 96/6 = 16MHz =&amp;gt; ADC0/1_CLK_PS[0:4] = 0b00010
    // =&amp;gt; ADC0/1_CR = 0x8002

    PUSH_TO_CFIFO1_A( B0                     |
                       ADC_REG_VALUE (0x8002) | // enables ADC0
                       ADC_REG_ADDR (ADC0_CR) );

    PUSH_TO_CFIFO1_A( EOQ                    |
                       B1                     |
                       ADC_REG_VALUE (0x8002) | // enables ADC1
                       ADC_REG_ADDR (ADC1_CR) );

    // Trigger CFIFO 0 using Single Scan SW mode
    SINGLE_SCAN_TRIGGER_Q1;


    // Wait for End Of Queue flag
    while (EQADC_A.FISR[1].B.EOQFX !=1)
    {
    }

    // Clear End Of Queue flag
    EQADC_A.FISR[1].R = FISR_EOQ_MASK;

    // eQADC calibration
    for(i=0;i&amp;lt;100000;i++) {}

    // note b05111: - this notation calls the function until it returns 0
    //              - would be probably better to use 'while' loop
    i=1;
    res=0;
    for(;i==1;i=EQADC_PowerUpCalibration())
    {
        res++;
    }

    D_UART_TransmitData("eqadc init\n",12);

}





int main(void)
{
	volatile int counter = 0;
	
	xcptn_xmpl ();              /* Configure and Enable Interrupts */


	// Hardware initialization
	    HW_init();

	    D_PLL_Init();

	    D_Init_eSCI_A ();
	    // eQADC initialization and calibration
	    eQADCA_init();




	/* Loop forever */
	for(;;) {	   

		PUSH_TO_CFIFO0_A( ANA29_command );

		        // Trigger CFIFO 0 using Single Scan SW mode
		        EQADC_A.CFCR0.B.MODE0 = SOFTWARE_TRIGGER_SINGLE_SCAN;
		        EQADC_A.CFCR0.B.SSE0 = 1;

		        // Wait for RFIFO 0's Drain Flag to set
		        while (EQADC_A.FISR[0].B.RFDFX != 1)
		        {
		        }

		        // Read conversion result
		        Result = POP_FROM_RFIFO0_A;

		        // Clear RFIFO 0's Drain Flag
		        EQADC_A.FISR[0].B.RFDFX = 1;

		        // Clear CFIFO's End of Queue flag
		        EQADC_A.FISR[0].B.EOQFX = 1;


		        // Display converted value
		        dec_to_str(str,(uint32_t)((5000*Result)/0x3FFC),5u);
		        	   	D_UART_TransmitData(str,5u);
		        	   	D_UART_TransmitData("\n",1);


	}
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 11:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1429255#M20682</guid>
      <dc:creator>Saidev</dc:creator>
      <dc:date>2022-03-16T11:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: EQADC output</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1430590#M20702</link>
      <description>&lt;P&gt;What is the voltage you are converting? Is it is stabilized output of laboratory power supply?&lt;/P&gt;
&lt;P&gt;Also you are converting without calibration, convert WITH calibration.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 08:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1430590#M20702</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-03-18T08:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: EQADC output</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1430723#M20707</link>
      <description>&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;I have some mVolt variations in my source, only when reading in CRO otherwise in multimeter it is showing constant voltage.&lt;/P&gt;&lt;P&gt;can you help me with how to program with calibration, what changes I have to make?&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 13:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1430723#M20707</guid>
      <dc:creator>Saidev</dc:creator>
      <dc:date>2022-03-18T13:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: EQADC output</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1431286#M20724</link>
      <description>&lt;P&gt;The example contains everything needed. Just use&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;PUSH_TO_CFIFO0_A( ANA29_command_cal );&lt;/LI-CODE&gt;
&lt;P&gt;instead of&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-c"&gt;&lt;CODE&gt;PUSH_TO_CFIFO0_A( ANA29_command );&lt;/CODE&gt;&lt;/PRE&gt;</description>
      <pubDate>Mon, 21 Mar 2022 12:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1431286#M20724</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-03-21T12:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: EQADC output</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1431864#M20735</link>
      <description>&lt;P&gt;Thanks for your reply,&lt;/P&gt;&lt;P&gt;Now I'm getting the closer output value, there is a 50mV variation in source that is what the issue earlier.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 09:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-output/m-p/1431864#M20735</guid>
      <dc:creator>Saidev</dc:creator>
      <dc:date>2022-03-22T09:45:45Z</dc:date>
    </item>
  </channel>
</rss>