<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックCould'nt enter IVOR6 Exception Handler</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1416874#M20487</link>
    <description>&lt;P&gt;Dear Mr. / Mrs.&lt;/P&gt;&lt;P&gt;I try to cause&amp;nbsp;illegal instruction exception by following source code on MPC5777C;&lt;/P&gt;&lt;P&gt;typedef void (*myfunc)();&lt;BR /&gt;myfunc foo = 0;&lt;BR /&gt;foo();&lt;/P&gt;&lt;P&gt;This shows that I am on right way.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20Sidar04_0-1645458429921.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171233iDE97BDE4655D9ED6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="20Sidar04_0-1645458429921.png" alt="20Sidar04_0-1645458429921.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As I see, when I tried debug my controller. My program is not stop on IVOR6_Exception_Handler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to handle this problem. I tried to cause IVOR6 exception for MPC5777C.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Feb 2022 15:52:36 GMT</pubDate>
    <dc:creator>20Sidar04</dc:creator>
    <dc:date>2022-02-21T15:52:36Z</dc:date>
    <item>
      <title>Could'nt enter IVOR6 Exception Handler</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1416874#M20487</link>
      <description>&lt;P&gt;Dear Mr. / Mrs.&lt;/P&gt;&lt;P&gt;I try to cause&amp;nbsp;illegal instruction exception by following source code on MPC5777C;&lt;/P&gt;&lt;P&gt;typedef void (*myfunc)();&lt;BR /&gt;myfunc foo = 0;&lt;BR /&gt;foo();&lt;/P&gt;&lt;P&gt;This shows that I am on right way.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20Sidar04_0-1645458429921.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171233iDE97BDE4655D9ED6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="20Sidar04_0-1645458429921.png" alt="20Sidar04_0-1645458429921.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As I see, when I tried debug my controller. My program is not stop on IVOR6_Exception_Handler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to handle this problem. I tried to cause IVOR6 exception for MPC5777C.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 15:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1416874#M20487</guid>
      <dc:creator>20Sidar04</dc:creator>
      <dc:date>2022-02-21T15:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: Could'nt enter IVOR6 Exception Handler</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1417336#M20496</link>
      <description>&lt;P&gt;se_illegal instruction (opcode 0x0000) then it depends if the device is running in debug mode or in standalone mode:&lt;/P&gt;
&lt;P&gt;- in debug mode, se_illegal works like software breakpoint. IVOR6 is not triggered. If you just step the code, it works like nop instruction. If you run the code and the program reaches se_illegal instruction, the device will stop execution and it will enter debug mode.&lt;/P&gt;
&lt;P&gt;- if the device is running in standalone without debugger, se_illegal will trigger IVOR6 exception.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 08:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1417336#M20496</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-02-22T08:51:33Z</dc:date>
    </item>
    <item>
      <title>Re: Could'nt enter IVOR6 Exception Handler</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1417495#M20503</link>
      <description>&lt;P&gt;Thanks David for advices. It works.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 12:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Could-nt-enter-IVOR6-Exception-Handler/m-p/1417495#M20503</guid>
      <dc:creator>20Sidar04</dc:creator>
      <dc:date>2022-02-22T12:52:46Z</dc:date>
    </item>
  </channel>
</rss>