<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5602P failed to flash in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399778#M20150</link>
    <description>&lt;P&gt;Hi David,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Noted that the delay after reset is the feature on MPC57xx devices.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We have the MCU on our PCB layout, it is not a dev board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jan 2022 01:28:59 GMT</pubDate>
    <dc:creator>JOE_1209</dc:creator>
    <dc:date>2022-01-17T01:28:59Z</dc:date>
    <item>
      <title>MPC5602P failed to flash</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399277#M20137</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried flashing a new project for the chip SPC5602PEF0VLH6, and failed. Please find the attached word file for detail. (&lt;/SPAN&gt;&lt;SPAN&gt;S32D Power Architecture MP5602P project.docx&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I came across this post: &lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DEVKIT-MPC5744P-Error-in-ONCE-status-register-during-instruction/m-p/866556#:~:text=In%20general%2C%20the%20message%20%22Error%20in%20ONCE%20status,has%20occurred%20bad%20signal%20due%20to%20bad%20hardware" target="_blank" rel="noopener"&gt;DEVKIT MPC5744P - Error in ONCE status register du... - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;where NXP guy mentioned:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In general, the message "Error in ONCE status register during instruction execution" means that the connection&amp;nbsp;between the P&amp;amp;E interface and the MPC5744 chip has been lost during the download process due to multiple possible causes like:&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;debug shift frequency being too high&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;a RESET has occurred&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;bad signal due to bad hardware&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since I have the same error message, I had different configurations of slowing down debug shift frequency(kHz) to 3000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;amp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Delay after reset and before communicating to target 200 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;which also does not work. Could bad signal be the only left cause here?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Joe&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 06:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399277#M20137</guid>
      <dc:creator>JOE_1209</dc:creator>
      <dc:date>2022-01-14T06:00:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5602P failed to flash</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399422#M20144</link>
      <description>&lt;P&gt;Hi, mentioned delay after reset was mainly due to reset escalation feature that is only present on MPC57xx devices.&lt;/P&gt;
&lt;P&gt;Actually which board you are using? You have only specified used MCU.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 10:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399422#M20144</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-01-14T10:14:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5602P failed to flash</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399778#M20150</link>
      <description>&lt;P&gt;Hi David,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Noted that the delay after reset is the feature on MPC57xx devices.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We have the MCU on our PCB layout, it is not a dev board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 01:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1399778#M20150</guid>
      <dc:creator>JOE_1209</dc:creator>
      <dc:date>2022-01-17T01:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5602P failed to flash</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1400267#M20158</link>
      <description>&lt;P&gt;Have you ever run this board? Have you checked power-up sequence i.e. voltage levels?&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 11:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5602P-failed-to-flash/m-p/1400267#M20158</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-01-17T11:46:53Z</dc:date>
    </item>
  </channel>
</rss>