<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMPC5554 EMIOS programmable input filter implementation question</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-EMIOS-programmable-input-filter-implementation-question/m-p/472288#M2015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a general question on how to implement a EMIOS programmable input filter for the MPC5554.&lt;/P&gt;&lt;P&gt;Using the assumptions:&lt;/P&gt;&lt;P&gt;1. A system clock frequency of 132MHz.&lt;/P&gt;&lt;P&gt;2. GPREN = 0x1, enabling the global clock prescalar.&lt;/P&gt;&lt;P&gt;3. GPRE[7:0] = 0x00000010, setting the global clock prescalar value to 3.&lt;/P&gt;&lt;P&gt;4. UCPREN = 0x1, enabling the unified channel prescalar&lt;/P&gt;&lt;P&gt;5. UCPRE[1:0]= 0x11, setting the clock divider value to 4. &lt;/P&gt;&lt;P&gt;6. FCK=0x0 so is set to prescaled clock.&lt;/P&gt;&lt;P&gt;7. IF=0x1000 (16 clock filter periods).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt; In the MPC5554 reference manual in figure 17-13 it shows the "Prescaled Clock" input. Is this the same input as the "prescaled clock" output seen in figure 17-54? If it is, then using the Ratio they show in figure 17-54, is (3*4)=12. Would the clock for the EMIOS then be prescaled down by 12, giving a programmed filter time of: 1/(132MHz)*12*16=1.45us?&lt;/P&gt;&lt;P&gt;I ask because my interpretation does not match up clearly to figure 17-12 which has a "internal counter clock" input to the unified prescalar and figure 17-1 which has the "system clock" going to a clock prescalar block.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jun 2016 20:23:45 GMT</pubDate>
    <dc:creator>ryanbeitlich</dc:creator>
    <dc:date>2016-06-01T20:23:45Z</dc:date>
    <item>
      <title>MPC5554 EMIOS programmable input filter implementation question</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-EMIOS-programmable-input-filter-implementation-question/m-p/472288#M2015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a general question on how to implement a EMIOS programmable input filter for the MPC5554.&lt;/P&gt;&lt;P&gt;Using the assumptions:&lt;/P&gt;&lt;P&gt;1. A system clock frequency of 132MHz.&lt;/P&gt;&lt;P&gt;2. GPREN = 0x1, enabling the global clock prescalar.&lt;/P&gt;&lt;P&gt;3. GPRE[7:0] = 0x00000010, setting the global clock prescalar value to 3.&lt;/P&gt;&lt;P&gt;4. UCPREN = 0x1, enabling the unified channel prescalar&lt;/P&gt;&lt;P&gt;5. UCPRE[1:0]= 0x11, setting the clock divider value to 4. &lt;/P&gt;&lt;P&gt;6. FCK=0x0 so is set to prescaled clock.&lt;/P&gt;&lt;P&gt;7. IF=0x1000 (16 clock filter periods).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt; In the MPC5554 reference manual in figure 17-13 it shows the "Prescaled Clock" input. Is this the same input as the "prescaled clock" output seen in figure 17-54? If it is, then using the Ratio they show in figure 17-54, is (3*4)=12. Would the clock for the EMIOS then be prescaled down by 12, giving a programmed filter time of: 1/(132MHz)*12*16=1.45us?&lt;/P&gt;&lt;P&gt;I ask because my interpretation does not match up clearly to figure 17-12 which has a "internal counter clock" input to the unified prescalar and figure 17-1 which has the "system clock" going to a clock prescalar block.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 20:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-EMIOS-programmable-input-filter-implementation-question/m-p/472288#M2015</guid>
      <dc:creator>ryanbeitlich</dc:creator>
      <dc:date>2016-06-01T20:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5554 EMIOS programmable input filter implementation question</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5554-EMIOS-programmable-input-filter-implementation-question/m-p/472289#M2016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;The Global Clock Prescaler (MCR[GPRE]) divides the System clock to generate an Internal Counter Clock for the clock prescalers of the unified channels, see Fig 17-1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;This Internal Counter Clock can be further divided by channel Prescaler (CCR[UCPRE]) so channel counts at Prescaler Clock, see Fig 17-12 and Fig 17-54. This Prescaler Clock can be also selected as clock source for programmable input filter.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 06:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5554-EMIOS-programmable-input-filter-implementation-question/m-p/472289#M2016</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-06-02T06:48:13Z</dc:date>
    </item>
  </channel>
</rss>