<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックFATFS not updating timestamp</title>
    <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1399056#M20133</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using SDK 3.0.3 With the FreeRTOS, FATFS and the RTC. I have the FATFS get the timestamp from the RTC module. The problem is the timestamp doesn't get updated instead it uses g_timeStampStartTime. Is there something special I need to do to have the timestamp in the FATFS to get updated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jan 2022 19:33:23 GMT</pubDate>
    <dc:creator>MattJCole</dc:creator>
    <dc:date>2022-01-13T19:33:23Z</dc:date>
    <item>
      <title>FATFS not updating timestamp</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1399056#M20133</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using SDK 3.0.3 With the FreeRTOS, FATFS and the RTC. I have the FATFS get the timestamp from the RTC module. The problem is the timestamp doesn't get updated instead it uses g_timeStampStartTime. Is there something special I need to do to have the timestamp in the FATFS to get updated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 19:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1399056#M20133</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2022-01-13T19:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: FATFS not updating timestamp</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1400926#M20169</link>
      <description>&lt;P&gt;Hi Matt,&lt;/P&gt;
&lt;P&gt;I can't see anything special. Could you check if this code is executed as expected?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1642507083005.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167977i9F59AAAD39B404E9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1642507083005.png" alt="lukaszadrapa_0-1642507083005.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 11:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1400926#M20169</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-01-18T11:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: FATFS not updating timestamp</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1402903#M20212</link>
      <description>&lt;P&gt;That code only initializes the timestamp when you mount the drive. after that the timestamp never gets updated. The function&amp;nbsp;TimeStamp_UpdateTimeDate just return&amp;nbsp;&lt;SPAN&gt;g_timeStampStartTime. There is a function called&amp;nbsp;TimeStamp_IRQHandler that does update&amp;nbsp; g_timeStampStartTime by calling the&amp;nbsp;TimeStamp_GetTimeDate function but it is never called.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 23:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1402903#M20212</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2022-01-20T23:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: FATFS not updating timestamp</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1405004#M20245</link>
      <description>&lt;P&gt;Ok and when you check the RTC module later, is it running and is the RTCF interrupt flag set?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 08:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1405004#M20245</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-01-26T08:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: FATFS not updating timestamp</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1405492#M20261</link>
      <description>&lt;P&gt;I did not do anything with the RTC module am I supposed to do somethin with it? I assumed the FATFS module would have handled that since it starts the RTC module and sets the date and time.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 18:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FATFS-not-updating-timestamp/m-p/1405492#M20261</guid>
      <dc:creator>MattJCole</dc:creator>
      <dc:date>2022-01-26T18:41:28Z</dc:date>
    </item>
  </channel>
</rss>