<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug error MPC5777c in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1397915#M20116</link>
    <description>&lt;P&gt;It is your own prototype board, correct? Do you have multiple boards? Do all facing the same issue? Also share details about use MCU (all 3 lines printed on the chip).&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 07:53:58 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2022-01-12T07:53:58Z</dc:date>
    <item>
      <title>Debug error MPC5777c</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395447#M20067</link>
      <description>&lt;P&gt;I'm getting error as in attached picture. I'm using MPC5777C controller, S32DS v1.2, USB multilink universal Rev C. My MCU external oscillator frequency is 40MHz. And SN74CBTLV3861PW for interfacing JTAG with MPC5777C. Please help.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 07:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395447#M20067</guid>
      <dc:creator>San_96</dc:creator>
      <dc:date>2022-01-06T07:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: Debug error MPC5777c</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395535#M20070</link>
      <description>&lt;P&gt;Have you ever get it to run or the issue happens with first time usage?&lt;/P&gt;
&lt;P&gt;Debugger cannot distinguish whether device is censored or JTAG communication just cannot be establish due to other reason, due to that warning says both options.&lt;/P&gt;
&lt;P&gt;Typically this warning is shown when device is powered-off (no power supply attached).&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 09:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395535#M20070</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-01-06T09:50:34Z</dc:date>
    </item>
    <item>
      <title>Re: Debug error MPC5777c</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395582#M20071</link>
      <description>&lt;P&gt;This is the new card. I've done the preliminary checking and verified the voltage supplies and frequencies on the board. All are seems to be okay.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the power supply is off and I'm running the debug, it is showing a warning as Device not detected or may be censored. Later it is showing the popup as in previous picture.&lt;/P&gt;&lt;P&gt;But when i provide power supply and I'm running the debug, it is directly showing popup as in previous picture.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 11:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1395582#M20071</guid>
      <dc:creator>San_96</dc:creator>
      <dc:date>2022-01-06T11:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: Debug error MPC5777c</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1397915#M20116</link>
      <description>&lt;P&gt;It is your own prototype board, correct? Do you have multiple boards? Do all facing the same issue? Also share details about use MCU (all 3 lines printed on the chip).&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 07:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Debug-error-MPC5777c/m-p/1397915#M20116</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-01-12T07:53:58Z</dc:date>
    </item>
  </channel>
</rss>