<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 MPC5606B invalid RCHW</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1387625#M19901</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've programmed an MPC5606B chip to use the private password &amp;amp; censorship turned on. However, the chip was still empty, so has an invalid RCHW and reset vector. Now, the BAM code seems to run &amp;amp; download through serial, but for any possible password. Then it seems to go into static state, or at least does not run or execute the downloaded BAM code.&lt;/P&gt;&lt;P&gt;Is there any way I can recover this chip?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;</description>
    <pubDate>Wed, 15 Dec 2021 22:31:51 GMT</pubDate>
    <dc:creator>jan_vdh</dc:creator>
    <dc:date>2021-12-15T22:31:51Z</dc:date>
    <item>
      <title>MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1387625#M19901</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've programmed an MPC5606B chip to use the private password &amp;amp; censorship turned on. However, the chip was still empty, so has an invalid RCHW and reset vector. Now, the BAM code seems to run &amp;amp; download through serial, but for any possible password. Then it seems to go into static state, or at least does not run or execute the downloaded BAM code.&lt;/P&gt;&lt;P&gt;Is there any way I can recover this chip?&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 22:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1387625#M19901</guid>
      <dc:creator>jan_vdh</dc:creator>
      <dc:date>2021-12-15T22:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1388241#M19913</link>
      <description>&lt;P&gt;Here you may see example codes for censorship on this device:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5604B-Censorship-CW210/ta-p/1123992" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5604B-Censorship-CW210/ta-p/1123992&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Common issue could be that password needs to be entered in reverse order i.e. 0xCAFE_BEEF_FEED_FACE (for private password 0xFEED_FACE_CAFE_BEEF).&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 16:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1388241#M19913</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-12-16T16:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1388920#M19933</link>
      <description>&lt;P&gt;&amp;nbsp;Thanks for the reply. That explained the weird behavior . One more question - once a chip is configured as public pw &amp;amp; censored, but I know the private password, can I still disable the censorship in the BAM bootloader by writing the private password to the PWCMPH &amp;amp; PWCMPL registers?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 16:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1388920#M19933</guid>
      <dc:creator>jan_vdh</dc:creator>
      <dc:date>2021-12-17T16:49:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1389496#M19941</link>
      <description>&lt;P&gt;Yes, you can &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="cs" data-phrase-index="0" data-number-of-phrases="1"&gt;&lt;SPAN&gt;temporarily&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt; disable censorship (until next reset) by entering the password over serial boot communication, here again in reverse order.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Dec 2021 10:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1389496#M19941</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-12-20T10:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1389656#M19946</link>
      <description>&lt;P&gt;Am I wrong to think that the chip only accepts the public password (feedface cafebeef) during the serial boot communication when configured to use the public password? I'm wondering if I can still somehow uncensor the chip in that configuration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 20 Dec 2021 19:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1389656#M19946</guid>
      <dc:creator>jan_vdh</dc:creator>
      <dc:date>2021-12-20T19:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1390722#M19962</link>
      <description>&lt;P&gt;If configured for public password, you are entering public password. If private password, then you are entering private password.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1640166761461.png" style="width: 614px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165966iFB25FE9FCCDF8508/image-dimensions/614x582?v=v2" width="614" height="582" role="button" title="davidtosenovjan_0-1640166761461.png" alt="davidtosenovjan_0-1640166761461.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 09:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1390722#M19962</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-12-22T09:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1390865#M19966</link>
      <description>&lt;P&gt;Thank you for the reply. The scenario I'm dealing with is as following:&lt;/P&gt;&lt;P&gt;* The chip is configured to use public password &amp;amp; is censored.&lt;/P&gt;&lt;P&gt;After entering the public password I can execute the BAM code. Now I'm wondering if the downloaded BAM code can disable censorship by writing the private password to the PWCMPH and PWCMPL registers?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Dec 2021 17:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1390865#M19966</guid>
      <dc:creator>jan_vdh</dc:creator>
      <dc:date>2021-12-22T17:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B invalid RCHW</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1391319#M19971</link>
      <description>&lt;P&gt;No, what you are describing is lock out. In this case MCU is censored forever.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1640254083372.png" style="width: 657px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166076i42E827DF4F753250/image-dimensions/657x631?v=v2" width="657" height="631" role="button" title="davidtosenovjan_0-1640254083372.png" alt="davidtosenovjan_0-1640254083372.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 10:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-invalid-RCHW/m-p/1391319#M19971</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-12-23T10:09:05Z</dc:date>
    </item>
  </channel>
</rss>